<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックLWIP IPV6 example</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LWIP-IPV6-example/m-p/846859#M50973</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying the double stack option with LWIP. The local link address is replying to the ping.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I try to add the lines&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IP6_ADDR(ip_2_ip6(&amp;amp;(fsl_netif0.ip6_addr[1])), 0xc30600fc, 0x91a853c3, 0x0, 0x04000000 );&lt;BR /&gt; IP_SET_TYPE_VAL(fsl_netif0.ip6_addr[1], IPADDR_TYPE_V6);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suppose the address will be added to the auto configured.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ping -6 fc00:6c3:c353:a891::4&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;does not get a reply. Is there something wrong in the added lines for setting the pinged address, or I should do more than this....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Help needed..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 Aug 2018 14:09:24 GMT</pubDate>
    <dc:creator>pietrodicastri</dc:creator>
    <dc:date>2018-08-31T14:09:24Z</dc:date>
    <item>
      <title>LWIP IPV6 example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LWIP-IPV6-example/m-p/846859#M50973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying the double stack option with LWIP. The local link address is replying to the ping.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I try to add the lines&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IP6_ADDR(ip_2_ip6(&amp;amp;(fsl_netif0.ip6_addr[1])), 0xc30600fc, 0x91a853c3, 0x0, 0x04000000 );&lt;BR /&gt; IP_SET_TYPE_VAL(fsl_netif0.ip6_addr[1], IPADDR_TYPE_V6);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suppose the address will be added to the auto configured.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ping -6 fc00:6c3:c353:a891::4&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;does not get a reply. Is there something wrong in the added lines for setting the pinged address, or I should do more than this....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Help needed..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Aug 2018 14:09:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LWIP-IPV6-example/m-p/846859#M50973</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2018-08-31T14:09:24Z</dc:date>
    </item>
  </channel>
</rss>