<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 KL24Z32VFT4 programming issue via FRDM-KL25Z OpenSDA</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL24Z32VFT4-programming-issue-via-FRDM-KL25Z-OpenSDA/m-p/842307#M50794</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;I tried to program my custom board which has KL24Z32VFT4 processor using FRDM-KL25Z as debugger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used&amp;nbsp;MSD-DEBUG-FRDM-KL25Z_Pemicro_v118.SDA as an OpenSDA firmware. But it did not program. But then I tried to debug another FRDM-KL25Z board using another FRDM-KL25Z board. I connected J6 connectors on the both FRDM boards and I was able to program. So that's mean Can't I use&amp;nbsp;&lt;SPAN&gt;MSD-DEBUG-FRDM-KL25Z_Pemicro_v118.SDA firmware to program&amp;nbsp;KL24Z32VFT4? Is it only support for&amp;nbsp;KL25Z?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks&lt;BR /&gt;Harsha&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Oct 2018 21:29:25 GMT</pubDate>
    <dc:creator>hb0038</dc:creator>
    <dc:date>2018-10-26T21:29:25Z</dc:date>
    <item>
      <title>KL24Z32VFT4 programming issue via FRDM-KL25Z OpenSDA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL24Z32VFT4-programming-issue-via-FRDM-KL25Z-OpenSDA/m-p/842307#M50794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;I tried to program my custom board which has KL24Z32VFT4 processor using FRDM-KL25Z as debugger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used&amp;nbsp;MSD-DEBUG-FRDM-KL25Z_Pemicro_v118.SDA as an OpenSDA firmware. But it did not program. But then I tried to debug another FRDM-KL25Z board using another FRDM-KL25Z board. I connected J6 connectors on the both FRDM boards and I was able to program. So that's mean Can't I use&amp;nbsp;&lt;SPAN&gt;MSD-DEBUG-FRDM-KL25Z_Pemicro_v118.SDA firmware to program&amp;nbsp;KL24Z32VFT4? Is it only support for&amp;nbsp;KL25Z?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks&lt;BR /&gt;Harsha&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Oct 2018 21:29:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL24Z32VFT4-programming-issue-via-FRDM-KL25Z-OpenSDA/m-p/842307#M50794</guid>
      <dc:creator>hb0038</dc:creator>
      <dc:date>2018-10-26T21:29:25Z</dc:date>
    </item>
    <item>
      <title>Re: KL24Z32VFT4 programming issue via FRDM-KL25Z OpenSDA</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL24Z32VFT4-programming-issue-via-FRDM-KL25Z-OpenSDA/m-p/842308#M50795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, you only can program the same microcontroller that way (see &lt;A href="https://community.nxp.com/thread/487068"&gt;Programming MKL24Z32VFT4 &lt;/A&gt;&amp;nbsp; and especially &lt;A class="link-titled" href="https://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/" title="https://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/"&gt;Using the Freedom Board as SWD Programmer | MCU on Eclipse&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;Keep in mind that MSD programming is more of a 'demo' feature, as programming speed will degrade over time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 27 Oct 2018 06:49:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL24Z32VFT4-programming-issue-via-FRDM-KL25Z-OpenSDA/m-p/842308#M50795</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2018-10-27T06:49:34Z</dc:date>
    </item>
  </channel>
</rss>