<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KEAZ-128Q80M- BOOTLOADER in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ-128Q80M-BOOTLOADER/m-p/841391#M50749</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David Maciel&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FRDM-KEAZ128Q80M does not have a bootloader into the chip, you can only program it through the OpenSDA interface (with the MSD flash programmer or with an IDE and debugging) or using an external programmer with the SWD port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Jul 2018 23:57:21 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2018-07-26T23:57:21Z</dc:date>
    <item>
      <title>KEAZ-128Q80M- BOOTLOADER</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ-128Q80M-BOOTLOADER/m-p/841390#M50748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I purchased an FRDM-KEAZ128Q80M card, I noticed that the card has 03 recording modes:&lt;/P&gt;&lt;P&gt;1. Direct connection to the compiler, (in case I am using the S32 compiler), through debug mode.&lt;/P&gt;&lt;P&gt;2. USB recording via the openSDA interface.&lt;/P&gt;&lt;P&gt;3. Recording via bootloader, also through the flash drive, however I do not know which type of extension supports this recording directly. In other words through the bootloader how is the microcontroller recording done?&lt;/P&gt;&lt;P&gt;I have not found any information that objectively describes writing codes via bootloader. I will be very grateful for the contributions.&lt;/P&gt;&lt;P&gt;Tks in Advanced!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2018 23:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ-128Q80M-BOOTLOADER/m-p/841390#M50748</guid>
      <dc:creator>davidmaciel</dc:creator>
      <dc:date>2018-07-23T23:26:48Z</dc:date>
    </item>
    <item>
      <title>Re: KEAZ-128Q80M- BOOTLOADER</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ-128Q80M-BOOTLOADER/m-p/841391#M50749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David Maciel&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FRDM-KEAZ128Q80M does not have a bootloader into the chip, you can only program it through the OpenSDA interface (with the MSD flash programmer or with an IDE and debugging) or using an external programmer with the SWD port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jul 2018 23:57:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEAZ-128Q80M-BOOTLOADER/m-p/841391#M50749</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2018-07-26T23:57:21Z</dc:date>
    </item>
  </channel>
</rss>