<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Emwin with K70 series in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Emwin-with-K70-series/m-p/840256#M50698</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Am currently using K22 series microcontroller from kinetics with SSD1963 LCD controller. we are planning to use internal LCD controller instead of SSD1963. We have shortlisted K70 series microcontroller which has a internal LCD controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;whether Emwin can be used with K70&lt;/P&gt;&lt;P&gt;if yes then where will i get the emwin library for K70&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anuj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Sep 2018 07:13:23 GMT</pubDate>
    <dc:creator>anujtanksali</dc:creator>
    <dc:date>2018-09-19T07:13:23Z</dc:date>
    <item>
      <title>Emwin with K70 series</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Emwin-with-K70-series/m-p/840256#M50698</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Am currently using K22 series microcontroller from kinetics with SSD1963 LCD controller. we are planning to use internal LCD controller instead of SSD1963. We have shortlisted K70 series microcontroller which has a internal LCD controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;whether Emwin can be used with K70&lt;/P&gt;&lt;P&gt;if yes then where will i get the emwin library for K70&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anuj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Sep 2018 07:13:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Emwin-with-K70-series/m-p/840256#M50698</guid>
      <dc:creator>anujtanksali</dc:creator>
      <dc:date>2018-09-19T07:13:23Z</dc:date>
    </item>
    <item>
      <title>Re: Emwin with K70 series</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Emwin-with-K70-series/m-p/840257#M50699</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Anuj,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes you can use emwin on the K70. Please refer the following &lt;A href="https://www.nxp.com/pages/emwin-graphics-library:EMWIN-GRAPHICS-LIBRARY"&gt;link&lt;/A&gt;&amp;nbsp;to learn more about the license that we provide for the NXP&amp;nbsp;microcontrollers.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you have not made the change yet to the K70, I highly recommend you to check the LPC54628 MCU to replace your K22 instead of the K70. K70 is an old MCU, on the other hand LPC54628 is one of our newest&amp;nbsp;&lt;SPAN&gt;microcontrollers. The LPC&lt;/SPAN&gt;&amp;nbsp;also has an LCD controller and&amp;nbsp;the advantage is that this MCU has SDK which includes multiple examples of the emwin library.&amp;nbsp;&amp;nbsp;A good idea will be to get the development board for the LPC54628, to see if the LPC fits to your project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/lpc-cortex-m-mcus/lpc54000-series-cortex-m4-mcus/power-efficient-microcontrollers-mcus-with-advanced-peripherals-based-on-arm-cortex-m4-core:LPC546XX"&gt;Link to the LPC54628 page.&amp;nbsp;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/lpc-cortex-m-mcus/lpc54000-series-cortex-m4-mcus/lpcxpresso54628-development-board:OM13098"&gt;Link to the development board for the LPC54628.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Sep 2018 15:32:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Emwin-with-K70-series/m-p/840257#M50699</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-09-21T15:32:17Z</dc:date>
    </item>
  </channel>
</rss>