<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K60 8 bit only flex bus</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-8-bit-only-flex-bus/m-p/839669#M50690</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Nick,&lt;/P&gt;&lt;P&gt;I see that you want to use FlexBus of K60 to read/write FPGA, how many bytes do you want to access FPGA? it is related to the address pins you have to connected.&lt;/P&gt;&lt;P&gt;I think you have to connect the FB_AD[7:0](assume the byte size you access is less than 256), CLKOUT pin and FB_ALE, you can design a flip-flop to latch the low address lines, connect the&amp;nbsp; FB_OE, FB_CSx and FB_RW signal so that you can read/write the FPGA.&lt;/P&gt;&lt;P&gt;In conclusion, pls connect FB_AD[7:0],CLKOUT, FB_ALE,FB_OE, FB_CSx and FB_RW.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Jul 2018 08:33:27 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2018-07-23T08:33:27Z</dc:date>
    <item>
      <title>K60 8 bit only flex bus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-8-bit-only-flex-bus/m-p/839668#M50689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm looking into the details of a new HW design and I am planning on using the Flexbus in 8 bit multiplexed mode to connect to an FPGA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have no need to connect any more than the 8 multiplexed bits and support strobes and clock to the FPGA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any issues of not enabling the flexbus mode of the other 24 AD IOs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to use those IO for other purposes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jul 2018 19:51:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-8-bit-only-flex-bus/m-p/839668#M50689</guid>
      <dc:creator>norton256</dc:creator>
      <dc:date>2018-07-20T19:51:14Z</dc:date>
    </item>
    <item>
      <title>Re: K60 8 bit only flex bus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-8-bit-only-flex-bus/m-p/839669#M50690</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Nick,&lt;/P&gt;&lt;P&gt;I see that you want to use FlexBus of K60 to read/write FPGA, how many bytes do you want to access FPGA? it is related to the address pins you have to connected.&lt;/P&gt;&lt;P&gt;I think you have to connect the FB_AD[7:0](assume the byte size you access is less than 256), CLKOUT pin and FB_ALE, you can design a flip-flop to latch the low address lines, connect the&amp;nbsp; FB_OE, FB_CSx and FB_RW signal so that you can read/write the FPGA.&lt;/P&gt;&lt;P&gt;In conclusion, pls connect FB_AD[7:0],CLKOUT, FB_ALE,FB_OE, FB_CSx and FB_RW.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2018 08:33:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-8-bit-only-flex-bus/m-p/839669#M50690</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-07-23T08:33:27Z</dc:date>
    </item>
    <item>
      <title>Re: K60 8 bit only flex bus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-8-bit-only-flex-bus/m-p/839670#M50691</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All I don't even need a full8 bits of address for this particular design. Thank you for confirming pin usage. That is very helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2018 12:43:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-8-bit-only-flex-bus/m-p/839670#M50691</guid>
      <dc:creator>norton256</dc:creator>
      <dc:date>2018-07-23T12:43:11Z</dc:date>
    </item>
  </channel>
</rss>