<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKinetis KLx Low Power Modes with External 32kHz Crystal</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KLx-Low-Power-Modes-with-External-32kHz-Crystal/m-p/835952#M50524</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; border: 0px;"&gt;I am using a KL16 and currently using the 4Mhz Internal Reference Clock. However, in order to reduce current consumption I would like to switch to my 32kHz crystal.&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;Since 32 kHz is not fast enough for my calculations and timers, i need to enable the FLL. However, is it possible to use that mode in VLPR mode as again I want to minimise the current consumption as much as possible. Would that work in any of the low power modes or can I only run it in Normal Run Mode.&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;In sleep modes (VLLS), is it more efficient to use the 32kHz crystal or the dedicated Low Power timer running off the LPO.&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;Thanks!&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 01 Jul 2018 17:33:40 GMT</pubDate>
    <dc:creator>christhomas</dc:creator>
    <dc:date>2018-07-01T17:33:40Z</dc:date>
    <item>
      <title>Kinetis KLx Low Power Modes with External 32kHz Crystal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KLx-Low-Power-Modes-with-External-32kHz-Crystal/m-p/835952#M50524</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; border: 0px;"&gt;I am using a KL16 and currently using the 4Mhz Internal Reference Clock. However, in order to reduce current consumption I would like to switch to my 32kHz crystal.&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;Since 32 kHz is not fast enough for my calculations and timers, i need to enable the FLL. However, is it possible to use that mode in VLPR mode as again I want to minimise the current consumption as much as possible. Would that work in any of the low power modes or can I only run it in Normal Run Mode.&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;In sleep modes (VLLS), is it more efficient to use the 32kHz crystal or the dedicated Low Power timer running off the LPO.&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;Thanks!&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Jul 2018 17:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KLx-Low-Power-Modes-with-External-32kHz-Crystal/m-p/835952#M50524</guid>
      <dc:creator>christhomas</dc:creator>
      <dc:date>2018-07-01T17:33:40Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis KLx Low Power Modes with External 32kHz Crystal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KLx-Low-Power-Modes-with-External-32kHz-Crystal/m-p/835953#M50525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q1: is it possible to use that mode in VLPR mode as again I want to minimise the current consumption as much as possible.&lt;/P&gt;&lt;P&gt;A1: No. Only MCG modes BLPI and BLPE can be used in VLPR. You can find it in "Table 7-1. Chip power modes" of KL16P80M48SF4RM.&lt;/P&gt;&lt;P&gt;So if you want to use the external 32kHz crystal(BLPE), the frequency may not fast enough for your calculations and timers.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/64937i1D28A4FAD1E8F8E7/image-size/large?v=v2&amp;amp;px=999" title="Table 7-1. Chip power modes.png" alt="Table 7-1. Chip power modes.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2: Would that work in any of the low power modes or can I only run it in Normal Run Mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;A2: If you want to use the FEE mode(external 32k crystal with FLL), you can only run it in&amp;nbsp; Normal Run Mode&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/64934i234186FC935B17FC/image-size/large?v=v2&amp;amp;px=999" title="Table 7-2. Module operation in low power modes.png" alt="Table 7-2. Module operation in low power modes.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q3: In sleep modes (VLLS), is it more efficient to use the 32kHz crystal or the dedicated Low Power timer running off the LPO. &lt;BR /&gt;A3: You can find the IEREFSTEN32KHz in "Table 10. Low power mode peripheral adders".&lt;/P&gt;&lt;P&gt;The LPO is always ON in VLLS1 and VLLS3, and can only be OFF in VLLS0 mode.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/64935i067F23E25683C6F7/image-size/large?v=v2&amp;amp;px=999" title="Table 10. Low power mode peripheral adders.png" alt="Table 10. Low power mode peripheral adders.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jul 2018 09:24:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KLx-Low-Power-Modes-with-External-32kHz-Crystal/m-p/835953#M50525</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2018-07-05T09:24:26Z</dc:date>
    </item>
  </channel>
</rss>