<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic fsl_ftm.c/h missing in SDK Builder in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/fsl-ftm-c-h-missing-in-SDK-Builder/m-p/835726#M50516</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the MCUXpresso SDK Builder to dowload all the libraries for MKE04Z128VLD4 microcontroller.&lt;/P&gt;&lt;P&gt;I have dowloaded the generated ZIP file with all the libs and files.The name of this packet is SDK_2.4.1_MKE04Z128xxx4.&lt;/P&gt;&lt;P&gt;It is supposed I should find the file "fsl_ftm.c" inside the folder "SDK_2.4.1_MKE04Z128xxx4\devices\MKE04Z1284\drivers", but it is missing.&lt;/P&gt;&lt;P&gt;However, I tried the same with the MKE04Z8xxx4 (same microcontroller with different memory size) and after dowloading the ZIP file, the file "fsl_ftm.c" is there.&lt;/P&gt;&lt;P&gt;So, I think SDK Builder has some kind of error when it is generating the SDK archive for the device MKE04Z128VLD4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am going to use the "fsl_ftm.c" I got from MKE04Z8xxx4&amp;nbsp; SDK archive, because I guess it is going to work correctly. But I would like SDK Builder provide me the correct file without being forced to do this "tricks".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Nov 2018 11:29:59 GMT</pubDate>
    <dc:creator>hector_fernande</dc:creator>
    <dc:date>2018-11-14T11:29:59Z</dc:date>
    <item>
      <title>fsl_ftm.c/h missing in SDK Builder</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/fsl-ftm-c-h-missing-in-SDK-Builder/m-p/835726#M50516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the MCUXpresso SDK Builder to dowload all the libraries for MKE04Z128VLD4 microcontroller.&lt;/P&gt;&lt;P&gt;I have dowloaded the generated ZIP file with all the libs and files.The name of this packet is SDK_2.4.1_MKE04Z128xxx4.&lt;/P&gt;&lt;P&gt;It is supposed I should find the file "fsl_ftm.c" inside the folder "SDK_2.4.1_MKE04Z128xxx4\devices\MKE04Z1284\drivers", but it is missing.&lt;/P&gt;&lt;P&gt;However, I tried the same with the MKE04Z8xxx4 (same microcontroller with different memory size) and after dowloading the ZIP file, the file "fsl_ftm.c" is there.&lt;/P&gt;&lt;P&gt;So, I think SDK Builder has some kind of error when it is generating the SDK archive for the device MKE04Z128VLD4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am going to use the "fsl_ftm.c" I got from MKE04Z8xxx4&amp;nbsp; SDK archive, because I guess it is going to work correctly. But I would like SDK Builder provide me the correct file without being forced to do this "tricks".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2018 11:29:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/fsl-ftm-c-h-missing-in-SDK-Builder/m-p/835726#M50516</guid>
      <dc:creator>hector_fernande</dc:creator>
      <dc:date>2018-11-14T11:29:59Z</dc:date>
    </item>
    <item>
      <title>Re: fsl_ftm.c/h missing in SDK Builder</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/fsl-ftm-c-h-missing-in-SDK-Builder/m-p/835727#M50517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hector,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have reported this issue internally. Thanks a lot for your feedback!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 18:45:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/fsl-ftm-c-h-missing-in-SDK-Builder/m-p/835727#M50517</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2018-11-21T18:45:23Z</dc:date>
    </item>
  </channel>
</rss>