<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFDRM K66 pin assignment searchable table?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K66-pin-assignment-searchable-table/m-p/835588#M50509</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is the table in the K-66 reference manual, which begins on page 186, section 11.3.1&amp;nbsp;K66 Signal Multiplexing and Pin Assignments, available in a searchable/editable format such as .csv or .xls?&amp;nbsp; I understand how the pin assignments work, but using search function is difficult in the pdf format, and I'd like be able to add additional content. Please share if anyone has this available.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Jun 2018 16:50:07 GMT</pubDate>
    <dc:creator>pleary</dc:creator>
    <dc:date>2018-06-29T16:50:07Z</dc:date>
    <item>
      <title>FDRM K66 pin assignment searchable table?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K66-pin-assignment-searchable-table/m-p/835588#M50509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is the table in the K-66 reference manual, which begins on page 186, section 11.3.1&amp;nbsp;K66 Signal Multiplexing and Pin Assignments, available in a searchable/editable format such as .csv or .xls?&amp;nbsp; I understand how the pin assignments work, but using search function is difficult in the pdf format, and I'd like be able to add additional content. Please share if anyone has this available.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2018 16:50:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K66-pin-assignment-searchable-table/m-p/835588#M50509</guid>
      <dc:creator>pleary</dc:creator>
      <dc:date>2018-06-29T16:50:07Z</dc:date>
    </item>
    <item>
      <title>Re: FDRM K66 pin assignment searchable table?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K66-pin-assignment-searchable-table/m-p/835589#M50510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The uTasker project contains device simulations which include pin mux assignment. &lt;BR /&gt;That means that it includes tables (in code) that can also be used as input to spread sheets and such.&lt;/P&gt;&lt;P&gt;I have attached the file &lt;EM&gt;kinetis_port_K26_K65_K66.h&lt;/EM&gt; which has an array table of the assignments which you can probably use.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM style="color: #3366ff;"&gt;uTasker - for more performance and faster, cheaper product development&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2018 18:30:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K66-pin-assignment-searchable-table/m-p/835589#M50510</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-06-29T18:30:07Z</dc:date>
    </item>
  </channel>
</rss>