<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB_CLKIN Specificatin for K27 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CLKIN-Specificatin-for-K27/m-p/835153#M50496</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, a&lt;SPAN style="font-size: small;"&gt;ccording to USB 2.0 specification, USB Full Speed communication rate accepts a maximum deviation of ±2500 ppm (±0.25%). This is what you should consider when selecting OSC. We don't have requirements for the rise/fall time because our oscillator circuitry is robust enough to support different rise times. Anyway, from the experience, it is as below:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: small;"&gt;---For high speed clocks we would say ~5ns for rise-fall times&lt;BR /&gt; -- For above 40MHz&amp;nbsp; it would need to be ~3ns or faster&lt;BR /&gt; -- For frequencies below 1MHz it could be slower than 5ns&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Aug 2018 06:09:52 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2018-08-14T06:09:52Z</dc:date>
    <item>
      <title>USB_CLKIN Specificatin for K27</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CLKIN-Specificatin-for-K27/m-p/835150#M50493</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm considering to use USB_CLKIN(USB0_CLKIN) for USB FS OTG of K27.&lt;/P&gt;&lt;P&gt;I think that its required accuracy of clock frequency is 500ppm same as USB2.0 specification.&lt;/P&gt;&lt;P&gt;But I couldn't found its required specification of jitter, duty, rise-time and fall-time.&lt;/P&gt;&lt;P&gt;Could you tell me them?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;M.Kiniwa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Aug 2018 11:36:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CLKIN-Specificatin-for-K27/m-p/835150#M50493</guid>
      <dc:creator>masahirokiniwa</dc:creator>
      <dc:date>2018-08-09T11:36:48Z</dc:date>
    </item>
    <item>
      <title>Re: USB_CLKIN Specificatin for K27</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CLKIN-Specificatin-for-K27/m-p/835151#M50494</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First please look at this document on the USB clock source.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94592"&gt;Kinetis USB Clock Sources&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So if you are&lt;SPAN style="font-size: 10pt; font-family: arial, helvetica, sans-serif;"&gt; using the USB_CLKIN pin to inject a 48MHz clock the USB will operate correctly if the clock source itself meets the usb specificacion. Just be note that &lt;SPAN style="font-size: 10pt; font-family: Cambria, serif; color: #000000;"&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;FLL cannot be used to clock the USB module because it do not meet the USB specification.&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Aug 2018 05:01:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CLKIN-Specificatin-for-K27/m-p/835151#M50494</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2018-08-10T05:01:02Z</dc:date>
    </item>
    <item>
      <title>Re: USB_CLKIN Specificatin for K27</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CLKIN-Specificatin-for-K27/m-p/835152#M50495</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mr.Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;I couldn't look you attached link. I'm unauthorized for its link.&lt;/P&gt;&lt;P&gt;If I check the usb specification, should I find the Table7-9 Full-speed Source Electrical Characteristics of USB specification Rev.2.0?&lt;/P&gt;&lt;P&gt;It's written based on 12MHz, but USB_CLKIN require higher frequency 48MHz.&lt;/P&gt;&lt;P&gt;Can I convert their specs for 48MHz?&lt;/P&gt;&lt;P&gt;ex.) Rise Time min 4ns / max 20ns based on 12MHz -&amp;gt; min 1ns / max 5ns base on 48MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;M.Kiniwa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Aug 2018 09:40:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CLKIN-Specificatin-for-K27/m-p/835152#M50495</guid>
      <dc:creator>masahirokiniwa</dc:creator>
      <dc:date>2018-08-10T09:40:07Z</dc:date>
    </item>
    <item>
      <title>Re: USB_CLKIN Specificatin for K27</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CLKIN-Specificatin-for-K27/m-p/835153#M50496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, a&lt;SPAN style="font-size: small;"&gt;ccording to USB 2.0 specification, USB Full Speed communication rate accepts a maximum deviation of ±2500 ppm (±0.25%). This is what you should consider when selecting OSC. We don't have requirements for the rise/fall time because our oscillator circuitry is robust enough to support different rise times. Anyway, from the experience, it is as below:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: small;"&gt;---For high speed clocks we would say ~5ns for rise-fall times&lt;BR /&gt; -- For above 40MHz&amp;nbsp; it would need to be ~3ns or faster&lt;BR /&gt; -- For frequencies below 1MHz it could be slower than 5ns&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Aug 2018 06:09:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CLKIN-Specificatin-for-K27/m-p/835153#M50496</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2018-08-14T06:09:52Z</dc:date>
    </item>
  </channel>
</rss>