<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LIN UART Problem in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-UART-Problem/m-p/834602#M50457</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Xia,&lt;/P&gt;&lt;P&gt;I am sorry for the delay.&lt;/P&gt;&lt;P&gt;Regarding your issue, pls refer to the RXEDGIF bit description, the RXEDGIF bit is set once it detects active edge on RxD pin, it is cleared&amp;nbsp; by writing a 1 to the bit. But you write a 0 to the bit, that is why you can not clear it.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66847i929D99089FBA2963/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Nov 2018 06:24:07 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2018-11-01T06:24:07Z</dc:date>
    <item>
      <title>LIN UART Problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-UART-Problem/m-p/834601#M50456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73986i84FC119B037E80EE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when I use the lin 4.5.9 package as a slave node.&amp;nbsp; debug the code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;s this picture. set&amp;nbsp; UARTx_S2&amp;nbsp;&amp;nbsp;RXEDGIF bit can't clear this bit。&lt;/P&gt;&lt;P&gt;then return , so the LIN CAN'T WORK.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Oct 2018 02:48:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-UART-Problem/m-p/834601#M50456</guid>
      <dc:creator>xiabin</dc:creator>
      <dc:date>2018-10-07T02:48:43Z</dc:date>
    </item>
    <item>
      <title>Re: LIN UART Problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-UART-Problem/m-p/834602#M50457</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Xia,&lt;/P&gt;&lt;P&gt;I am sorry for the delay.&lt;/P&gt;&lt;P&gt;Regarding your issue, pls refer to the RXEDGIF bit description, the RXEDGIF bit is set once it detects active edge on RxD pin, it is cleared&amp;nbsp; by writing a 1 to the bit. But you write a 0 to the bit, that is why you can not clear it.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66847i929D99089FBA2963/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Nov 2018 06:24:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-UART-Problem/m-p/834602#M50457</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-11-01T06:24:07Z</dc:date>
    </item>
  </channel>
</rss>