<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Kinetis K64F /K66F code licence for SDCard/MMC  in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-K66F-code-licence-for-SDCard-MMC/m-p/834470#M50445</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Kerry for the confirmation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am planning to use the SD Card code along with USB. So, I will use most of the code along with my application.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am glad that I do not need to pay for SD Card code that are used in K64 or K66 examples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mahendran.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Jul 2018 00:28:26 GMT</pubDate>
    <dc:creator>mahendranmanoha</dc:creator>
    <dc:date>2018-07-12T00:28:26Z</dc:date>
    <item>
      <title>Kinetis K64F /K66F code licence for SDCard/MMC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-K66F-code-licence-for-SDCard-MMC/m-p/834468#M50443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am planning to use the&amp;nbsp;sample code in my small project from KSDK example projects such as "usb_examples_dev_msc_sdcard_bm".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am wondering if this code is generic to both SD and MMC card or does this code also contains SDCard specific licensed code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In simple terms, do I need to pay a license fee if I use this code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Mahendran.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Jul 2018 02:20:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-K66F-code-licence-for-SDCard-MMC/m-p/834468#M50443</guid>
      <dc:creator>mahendranmanoha</dc:creator>
      <dc:date>2018-07-01T02:20:19Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64F /K66F code licence for SDCard/MMC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-K66F-code-licence-for-SDCard-MMC/m-p/834469#M50444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mahendran,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; All the code in the SDK which you downloaded from nxp official website, you can use it, it's no problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If you just want to use the SD and MMC driver, not the usb code, I suggest you use the middleware driver, take K64 sdk as an example, you can find the sdmmc driver from this folder:&lt;/P&gt;&lt;P&gt;SDK_2.2_TWR-K64F120M\middleware\sdmmc_2.1.2&lt;/P&gt;&lt;P&gt;Please check you SDK package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Jul 2018 08:52:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-K66F-code-licence-for-SDCard-MMC/m-p/834469#M50444</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-07-02T08:52:52Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64F /K66F code licence for SDCard/MMC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-K66F-code-licence-for-SDCard-MMC/m-p/834470#M50445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Kerry for the confirmation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am planning to use the SD Card code along with USB. So, I will use most of the code along with my application.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am glad that I do not need to pay for SD Card code that are used in K64 or K66 examples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mahendran.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2018 00:28:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-K66F-code-licence-for-SDCard-MMC/m-p/834470#M50445</guid>
      <dc:creator>mahendranmanoha</dc:creator>
      <dc:date>2018-07-12T00:28:26Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64F /K66F code licence for SDCard/MMC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-K66F-code-licence-for-SDCard-MMC/m-p/834471#M50446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are welcome.&lt;/P&gt;&lt;P&gt;&amp;nbsp;All the SDK code which you can downloaded from our nxp website is free, feel free to use it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2018 03:14:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64F-K66F-code-licence-for-SDCard-MMC/m-p/834471#M50446</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-07-12T03:14:17Z</dc:date>
    </item>
  </channel>
</rss>