<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Setting IPv4 of tower kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-IPv4-of-tower-kit/m-p/833447#M50408</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanx for ur quick response Daniel. Actually, I haven't used shell commands with microcontrollers. I've used them like initialize or setting up microcontroller through main() function. I am struggling with it since last week. If u can prove me any sample project then it would be a great help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Sep 2018 14:01:07 GMT</pubDate>
    <dc:creator>prashantdev</dc:creator>
    <dc:date>2018-09-18T14:01:07Z</dc:date>
    <item>
      <title>Setting IPv4 of tower kit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-IPv4-of-tower-kit/m-p/833445#M50406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using k60 tower kit. I've fnet stack for my application and I am not using any RTOS. Can anyone help me in setting the ipv4 address for my board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Sep 2018 05:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-IPv4-of-tower-kit/m-p/833445#M50406</guid>
      <dc:creator>prashantdev</dc:creator>
      <dc:date>2018-09-18T05:04:47Z</dc:date>
    </item>
    <item>
      <title>Re: Setting IPv4 of tower kit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-IPv4-of-tower-kit/m-p/833446#M50407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;HI Prashant:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are using FNET, I would suggest you refer to the FNET quick start guider.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Ffnet.sourceforge.net%2Fmanual%2Fquick_start_shell.html" rel="nofollow noopener noreferrer" target="_blank"&gt;Embedded TCP/IP stack: FNET Shell Demo Quick Start&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;You are able to change the default network parameters manually:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;By using Shell commands:&lt;PRE class=""&gt;set address &amp;lt;default-if IPv4 address&amp;gt; set gateway &amp;lt;default-if IPv4 gateway address&amp;gt; set netmask &amp;lt;default-if IPv4 netmask address&amp;gt; set mac &amp;lt;default-if Ethernet address&amp;gt;&lt;/PRE&gt;&lt;/LI&gt;&lt;LI&gt;By changing the default values in the &lt;EM&gt;fapp_user_config.h&lt;/EM&gt; source file. &lt;BR /&gt; Your local system administrator is able to assign a unique IPv4 address for the board, and also provide you with the IPv4 addresses of the gateway and the netmask.&lt;/LI&gt;&lt;/UL&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Sep 2018 06:01:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-IPv4-of-tower-kit/m-p/833446#M50407</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2018-09-18T06:01:52Z</dc:date>
    </item>
    <item>
      <title>Re: Setting IPv4 of tower kit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-IPv4-of-tower-kit/m-p/833447#M50408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanx for ur quick response Daniel. Actually, I haven't used shell commands with microcontrollers. I've used them like initialize or setting up microcontroller through main() function. I am struggling with it since last week. If u can prove me any sample project then it would be a great help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Sep 2018 14:01:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-IPv4-of-tower-kit/m-p/833447#M50408</guid>
      <dc:creator>prashantdev</dc:creator>
      <dc:date>2018-09-18T14:01:07Z</dc:date>
    </item>
  </channel>
</rss>