<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックWhat is __gnu_thumb1_case_sqi ?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-gnu-thumb1-case-sqi/m-p/829946#M50188</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1.I had define an chip(KEA128) file of XXXX.ld,as follows:&lt;/P&gt;&lt;P&gt;/* Specify the memory areas */&lt;BR /&gt;MEMORY&lt;BR /&gt;{&lt;BR /&gt;XXXXXXX&lt;BR /&gt; m_text (rx) : ORIGIN = 0x00008C00, LENGTH = 128K - 0x8C00&lt;BR /&gt; XXXXXXX&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.and compiler to an file of XXX.map,One of the paragraphs below:&lt;/P&gt;&lt;P&gt;*(.text)&lt;BR /&gt; .text 0x00000a00 0x14 c:/freescale/cw mcu v10.7/cross_tools/arm-none-eabi-gcc-4_7_3/bin/../lib/gcc/arm-none-eabi/4.7.3/armv6-m\libgcc.a(_thumb1_case_sqi.o)&lt;BR /&gt; 0x00000a00 __gnu_thumb1_case_sqi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.and i make mistakes,let the data of address at 0xa00 had change.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4.and power off ==&amp;gt; power on,then the code still can run normal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;5.I want to ask&amp;nbsp;what is it of&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;__gnu_thumb1_case_sqi ,why this function had change,but look like the code is still run normal.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Sep 2018 11:17:22 GMT</pubDate>
    <dc:creator>billchang</dc:creator>
    <dc:date>2018-09-17T11:17:22Z</dc:date>
    <item>
      <title>What is __gnu_thumb1_case_sqi ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-gnu-thumb1-case-sqi/m-p/829946#M50188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1.I had define an chip(KEA128) file of XXXX.ld,as follows:&lt;/P&gt;&lt;P&gt;/* Specify the memory areas */&lt;BR /&gt;MEMORY&lt;BR /&gt;{&lt;BR /&gt;XXXXXXX&lt;BR /&gt; m_text (rx) : ORIGIN = 0x00008C00, LENGTH = 128K - 0x8C00&lt;BR /&gt; XXXXXXX&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.and compiler to an file of XXX.map,One of the paragraphs below:&lt;/P&gt;&lt;P&gt;*(.text)&lt;BR /&gt; .text 0x00000a00 0x14 c:/freescale/cw mcu v10.7/cross_tools/arm-none-eabi-gcc-4_7_3/bin/../lib/gcc/arm-none-eabi/4.7.3/armv6-m\libgcc.a(_thumb1_case_sqi.o)&lt;BR /&gt; 0x00000a00 __gnu_thumb1_case_sqi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.and i make mistakes,let the data of address at 0xa00 had change.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4.and power off ==&amp;gt; power on,then the code still can run normal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;5.I want to ask&amp;nbsp;what is it of&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;__gnu_thumb1_case_sqi ,why this function had change,but look like the code is still run normal.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Sep 2018 11:17:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-gnu-thumb1-case-sqi/m-p/829946#M50188</guid>
      <dc:creator>billchang</dc:creator>
      <dc:date>2018-09-17T11:17:22Z</dc:date>
    </item>
    <item>
      <title>Re: What is __gnu_thumb1_case_sqi ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-gnu-thumb1-case-sqi/m-p/829947#M50189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bill Chang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;libgcc is a library that below to the GCC, it provides a low-level runtime library which could handle arithmetic operations and it also includes routines for exception handling, and a handful of miscellaneous operations. We don't have access to this code as they are managed by the library.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Sep 2018 21:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-gnu-thumb1-case-sqi/m-p/829947#M50189</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2018-09-19T21:21:32Z</dc:date>
    </item>
  </channel>
</rss>