<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.mx rt1020 evk board a new project using keil  in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/i-mx-rt1020-evk-board-a-new-project-using-keil/m-p/829609#M50139</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I started to use i.mx rt1020 evk board and I try to create a new project using keil ,but there is always errors.&lt;/P&gt;&lt;P&gt;How can I create a new project on keil ?Is there any document in this topic?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Dec 2018 14:20:24 GMT</pubDate>
    <dc:creator>bilge_kara157</dc:creator>
    <dc:date>2018-12-24T14:20:24Z</dc:date>
    <item>
      <title>i.mx rt1020 evk board a new project using keil</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/i-mx-rt1020-evk-board-a-new-project-using-keil/m-p/829609#M50139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I started to use i.mx rt1020 evk board and I try to create a new project using keil ,but there is always errors.&lt;/P&gt;&lt;P&gt;How can I create a new project on keil ?Is there any document in this topic?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Dec 2018 14:20:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/i-mx-rt1020-evk-board-a-new-project-using-keil/m-p/829609#M50139</guid>
      <dc:creator>bilge_kara157</dc:creator>
      <dc:date>2018-12-24T14:20:24Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx rt1020 evk board a new project using keil</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/i-mx-rt1020-evk-board-a-new-project-using-keil/m-p/829610#M50140</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you need the i.MX forum rather than the Kinetis forum.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Dec 2018 23:24:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/i-mx-rt1020-evk-board-a-new-project-using-keil/m-p/829610#M50140</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-12-26T23:24:51Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx rt1020 evk board a new project using keil</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/i-mx-rt1020-evk-board-a-new-project-using-keil/m-p/829611#M50141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi bilge kara,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Last time, please create your I.MX RT question in the i.mx area:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/community/imx/content" title="https://community.nxp.com/community/imx/content"&gt;i.MX Processors&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; This time, I reply you directly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If you want to create the rt1020 keil project, I suggest you refer to the official SDK keil project, which can be downloaded from this link:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/welcome" title="https://mcuxpresso.nxp.com/en/welcome"&gt;Welcome | MCUXpresso SDK Builder&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Select the RT1020 processor, generate the code, and download it.&lt;/P&gt;&lt;P&gt;&amp;nbsp; You can refer to the simple project, eg: SDK_2.5.0_EVK-MIMXRT1020\boards\evkmimxrt1020\demo_apps\led_blinky\mdk&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If you just want to run it from RAM, you can use these files as the startup file:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/71102i6575A13AC82936C7/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; You can totally create a project which is the same as the KSDK, after add the files, in the options, you need to add the include paths:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/71158i2D4E6E9E055FDEA7/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please try it on your side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, you can create the new post in the I.MX area, then I will provide the detail support for you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Dec 2018 10:36:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/i-mx-rt1020-evk-board-a-new-project-using-keil/m-p/829611#M50141</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-12-27T10:36:07Z</dc:date>
    </item>
  </channel>
</rss>