<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Serial wire debug pin is pulled down/up internally.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Serial-wire-debug-pin-is-pulled-down-up-internally/m-p/828715#M50086</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;① internal 30 kΩ to 60 kΩ&lt;BR /&gt;② It does not have to pull up pulled down externally. But external pull resistors are recommended.&lt;BR /&gt;③ external 4.7 kΩ to 10 kΩ&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Dec 2018 08:51:31 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2018-12-04T08:51:31Z</dc:date>
    <item>
      <title>Serial wire debug pin is pulled down/up internally.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Serial-wire-debug-pin-is-pulled-down-up-internally/m-p/828714#M50085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please kindly advise.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about SWD hardware.&lt;/P&gt;&lt;P&gt;In the manual "Document Number: MKMxxZxxACxx5RM Rev. 1, 09/2014"&lt;BR /&gt;"9.2 Debug Port Pin Descriptions" has the following description.&lt;/P&gt;&lt;P&gt;Serial Wire Clock. This pin is the clock for debug logic when in Serial Wire Debug mode. This pin is pulled down internally.&lt;BR /&gt;Serial wire debug data input / output. The SWD_IO pin is used by an external debug tool for communication and device control.&lt;/P&gt;&lt;P&gt;There are SWD_CLK pull-down and SWD_IO pull-up.&lt;BR /&gt;I have a question about this.&lt;BR /&gt;① What is the value of this pull-up resistor and pull-down resistor?&lt;BR /&gt;② Does it not have to pull up pulled down externally?&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Or should I do it?&lt;BR /&gt;③ If the pull-up / pull-down is required, how much resistance?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not have good English.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Dec 2018 03:03:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Serial-wire-debug-pin-is-pulled-down-up-internally/m-p/828714#M50085</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2018-12-04T03:03:49Z</dc:date>
    </item>
    <item>
      <title>Re: Serial wire debug pin is pulled down/up internally.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Serial-wire-debug-pin-is-pulled-down-up-internally/m-p/828715#M50086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;① internal 30 kΩ to 60 kΩ&lt;BR /&gt;② It does not have to pull up pulled down externally. But external pull resistors are recommended.&lt;BR /&gt;③ external 4.7 kΩ to 10 kΩ&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Dec 2018 08:51:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Serial-wire-debug-pin-is-pulled-down-up-internally/m-p/828715#M50086</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2018-12-04T08:51:31Z</dc:date>
    </item>
  </channel>
</rss>