<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックGPIO input capture for both edge</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-input-capture-for-both-edge/m-p/231135#M4994</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear support, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We tried your hands on project on our TWR-MK60N512 and came across some strange phenomenon.&amp;nbsp; Apparently we could capture both edges of SW2 on GPIO2 configuration which links to PTE26 on PORTE.&amp;nbsp; However, if we tried to modify the code to let SW1 on GPIO1 which links to PTA19 on PORTA and capture both edges, somehow it cannot respond to the pressed button.&amp;nbsp; When we release the SW1 on the board, then GPIO1_OnPortEvent will be executed twice.&amp;nbsp; Is there a bug in the setting of GPIO1 which we neglect in the first place?&amp;nbsp; We even tried to create a GPIO init code to pull up PTA19 but it just keeps generating interrupt.&amp;nbsp; If you can help us to clarify he issue, that would be wonderful!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vincent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Jan 2013 10:07:46 GMT</pubDate>
    <dc:creator>vincentchou</dc:creator>
    <dc:date>2013-01-21T10:07:46Z</dc:date>
    <item>
      <title>GPIO input capture for both edge</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-input-capture-for-both-edge/m-p/231135#M4994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear support, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We tried your hands on project on our TWR-MK60N512 and came across some strange phenomenon.&amp;nbsp; Apparently we could capture both edges of SW2 on GPIO2 configuration which links to PTE26 on PORTE.&amp;nbsp; However, if we tried to modify the code to let SW1 on GPIO1 which links to PTA19 on PORTA and capture both edges, somehow it cannot respond to the pressed button.&amp;nbsp; When we release the SW1 on the board, then GPIO1_OnPortEvent will be executed twice.&amp;nbsp; Is there a bug in the setting of GPIO1 which we neglect in the first place?&amp;nbsp; We even tried to create a GPIO init code to pull up PTA19 but it just keeps generating interrupt.&amp;nbsp; If you can help us to clarify he issue, that would be wonderful!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vincent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jan 2013 10:07:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-input-capture-for-both-edge/m-p/231135#M4994</guid>
      <dc:creator>vincentchou</dc:creator>
      <dc:date>2013-01-21T10:07:46Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO input capture for both edge</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-input-capture-for-both-edge/m-p/231136#M4995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just a hardware thought (and not knowing anything about your configuration): could "switch bounce" cause these symptoms?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;G'luck&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2013 21:02:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-input-capture-for-both-edge/m-p/231136#M4995</guid>
      <dc:creator>injunear1</dc:creator>
      <dc:date>2013-01-25T21:02:09Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO input capture for both edge</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-input-capture-for-both-edge/m-p/231137#M4996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes!&amp;nbsp; It is possible that the problem originates from board issues.&amp;nbsp; We tried the same code on SW2 and it worked.&amp;nbsp; We also tried the code on TWRK60F120M and TWRK70F120M and both boards worked. I started to wonder our TWR-K60N512 has some problems.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vincent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2013 23:24:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-input-capture-for-both-edge/m-p/231137#M4996</guid>
      <dc:creator>vincentchou</dc:creator>
      <dc:date>2013-01-25T23:24:56Z</dc:date>
    </item>
  </channel>
</rss>