<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: FlexBus configuration question K20 - Mqx 4.0</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-configuration-question-K20-Mqx-4-0/m-p/231063#M4990</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I routed my FlexBus slightly differently on a K60 device but I guess the end result should be the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've got an SRAM device with 20 address pins and 16 data. I&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt; routed FB_AD[0-15] and FB_A[16-19] to the ADDR[0-19] signals and routed FB_AD[16-31] to my DATA[0-15] pins.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm hoping that I've got this configuration correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kev&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Aug 2013 09:59:47 GMT</pubDate>
    <dc:creator>weblar</dc:creator>
    <dc:date>2013-08-01T09:59:47Z</dc:date>
    <item>
      <title>FlexBus configuration question K20 - Mqx 4.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-configuration-question-K20-Mqx-4-0/m-p/231061#M4988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a simple question (I think) before we spin some boards I want to be sure about this. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem: I need to configure FlexBus to non-multiplex mode. My question is about assigning the address and data lines. &lt;/P&gt;&lt;P&gt;This is what I want to do:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assign AD0 to AD7 to be the 8 data lines.&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;Assign A16-A29 to be the 14 address lines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will this work? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a ton in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jul 2013 16:47:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-configuration-question-K20-Mqx-4-0/m-p/231061#M4988</guid>
      <dc:creator>cavebiker</dc:creator>
      <dc:date>2013-07-30T16:47:35Z</dc:date>
    </item>
    <item>
      <title>Re: FlexBus configuration question K20 - Mqx 4.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-configuration-question-K20-Mqx-4-0/m-p/231062#M4989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it looks like the boards are wired correctly based on what the K20 manual says:&lt;/P&gt;&lt;P&gt;&lt;STRONG style="color: red; font-size: 9.0pt; font-family: HelveticaLTStd-Bold;"&gt;Module signal name Description I/O&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt; font-family: HelveticaLTStd-Roman; color: red;"&gt;FB_AD[29:16] Address Bus When FlexBus is used in a nonmultiplexed configuration, this is the&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt; font-family: HelveticaLTStd-Roman; color: red;"&gt;address bus. &lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt; font-family: HelveticaLTStd-Roman; color: red;"&gt;FB_AD[31:0] When FlexBus is used in a nonmultiplexed configuration, this is the data bus, FB_D. &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jul 2013 15:24:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-configuration-question-K20-Mqx-4-0/m-p/231062#M4989</guid>
      <dc:creator>cavebiker</dc:creator>
      <dc:date>2013-07-31T15:24:55Z</dc:date>
    </item>
    <item>
      <title>Re: FlexBus configuration question K20 - Mqx 4.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-configuration-question-K20-Mqx-4-0/m-p/231063#M4990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I routed my FlexBus slightly differently on a K60 device but I guess the end result should be the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've got an SRAM device with 20 address pins and 16 data. I&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt; routed FB_AD[0-15] and FB_A[16-19] to the ADDR[0-19] signals and routed FB_AD[16-31] to my DATA[0-15] pins.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm hoping that I've got this configuration correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kev&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Aug 2013 09:59:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-configuration-question-K20-Mqx-4-0/m-p/231063#M4990</guid>
      <dc:creator>weblar</dc:creator>
      <dc:date>2013-08-01T09:59:47Z</dc:date>
    </item>
    <item>
      <title>Re: FlexBus configuration question K20 - Mqx 4.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-configuration-question-K20-Mqx-4-0/m-p/231064#M4991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That should work if I am reading the manual correctly. Good luck.&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Aug 2013 19:16:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-configuration-question-K20-Mqx-4-0/m-p/231064#M4991</guid>
      <dc:creator>cavebiker</dc:creator>
      <dc:date>2013-08-02T19:16:38Z</dc:date>
    </item>
    <item>
      <title>Re: FlexBus configuration question K20 - Mqx 4.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-configuration-question-K20-Mqx-4-0/m-p/231065#M4992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Kev,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did this work for you? I never got Flexbus working correctly in this configuration. My hardware team is telling me Freescale told them that it is wired wrong, so I just created the bus with I/O :smileyplain:. It works but we are re-spinning the board so we can use Flexbus. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2013 21:44:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-configuration-question-K20-Mqx-4-0/m-p/231065#M4992</guid>
      <dc:creator>cavebiker</dc:creator>
      <dc:date>2013-09-05T21:44:04Z</dc:date>
    </item>
    <item>
      <title>Re: FlexBus configuration question K20 - Mqx 4.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-configuration-question-K20-Mqx-4-0/m-p/231066#M4993</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry its taken so long to reply, I don't log on to this forum as often as I should.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yeah, my FlexBus is working perfectly - I've got an LCD and SRAM hooked up to the FB using different chip selects and both devices seem to work without issue. What was your exact pin mapping?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Kev&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Sep 2013 08:30:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-configuration-question-K20-Mqx-4-0/m-p/231066#M4993</guid>
      <dc:creator>weblar</dc:creator>
      <dc:date>2013-09-19T08:30:52Z</dc:date>
    </item>
  </channel>
</rss>