<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K82 : WDOG in LLS3 mode in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-WDOG-in-LLS3-mode/m-p/825362#M49886</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, yes this is a question, should I trust to one source of LLWU wakeup like LPTIMERx or second one like RTC is need to play "WDOG" role as well ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;May be external WDOG is need, MCU should wakeup from LLS3 periodically and by using GPIO pin refresh it.&lt;/P&gt;&lt;P&gt;It look as more reliable scheme for control MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Aug 2018 05:44:29 GMT</pubDate>
    <dc:creator>EugeneHiihtaja</dc:creator>
    <dc:date>2018-08-28T05:44:29Z</dc:date>
    <item>
      <title>K82 : WDOG in LLS3 mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-WDOG-in-LLS3-mode/m-p/825360#M49884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I keep K82 in LLS3 mode and wakeup periodically by using LPTIMER0.&lt;/P&gt;&lt;P&gt;For secure MCU execution flow and periodical wakeup, I also would like to use WDOG for reboot MCU if wakeup is not happens in time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But even I configure WDOG for be used in Stop Mode :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;config.clockSource = kWDOG_LpoClockSource; // 1ms&lt;BR /&gt; config.workMode.enableStop = true;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is NOT reboot MCU if it stay in LLS3 mode long time without update.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I understand WDOG functionality in wrong way ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or may be I should use RTOS timer in parallel ( as back up timer ) for wakeup MCU if LPTIMER0 is suddenly freeze&lt;/P&gt;&lt;P&gt;while MCU in LLS3 mode ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please give advice !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Aug 2018 12:42:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-WDOG-in-LLS3-mode/m-p/825360#M49884</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2018-08-27T12:42:18Z</dc:date>
    </item>
    <item>
      <title>Re: K82 : WDOG in LLS3 mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-WDOG-in-LLS3-mode/m-p/825361#M49885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eugene,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Yes, you understand the WDOG in the wrong way, please check these information:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67590i9AB982ECF0494B21/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67639iFF43031084CC7A20/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When you enter the LLS3 mode, you need to use the LLWU module to wake it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Aug 2018 05:23:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-WDOG-in-LLS3-mode/m-p/825361#M49885</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-08-28T05:23:01Z</dc:date>
    </item>
    <item>
      <title>Re: K82 : WDOG in LLS3 mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-WDOG-in-LLS3-mode/m-p/825362#M49886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, yes this is a question, should I trust to one source of LLWU wakeup like LPTIMERx or second one like RTC is need to play "WDOG" role as well ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;May be external WDOG is need, MCU should wakeup from LLS3 periodically and by using GPIO pin refresh it.&lt;/P&gt;&lt;P&gt;It look as more reliable scheme for control MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Aug 2018 05:44:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-WDOG-in-LLS3-mode/m-p/825362#M49886</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2018-08-28T05:44:29Z</dc:date>
    </item>
    <item>
      <title>Re: K82 : WDOG in LLS3 mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-WDOG-in-LLS3-mode/m-p/825363#M49887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eugene,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can use more than one wakeup source in LLWU, please check the following information:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67830i624D04D10E0ED71E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67876i1F7F9E72E4B4DD1D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So, you can use both the LPTMR and RTC, or the GPIO as the LLWU wake up source.&lt;/P&gt;&lt;P&gt;It's OK.&lt;/P&gt;&lt;P&gt;More detail, please check the LLWU chapter in the chip reference manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Aug 2018 06:27:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-WDOG-in-LLS3-mode/m-p/825363#M49887</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-08-28T06:27:06Z</dc:date>
    </item>
  </channel>
</rss>