<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックOpen drain output pin on KL25Z?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Open-drain-output-pin-on-KL25Z/m-p/230817#M4967</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How should I do to set a GPIO output pin as open drain?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There seems to be no option for that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or should I set the GPIO as input when I want to set the pin high and set the GPIO as low output when I want to set the pin low?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Jun 2013 13:56:26 GMT</pubDate>
    <dc:creator>markosiponen</dc:creator>
    <dc:date>2013-06-20T13:56:26Z</dc:date>
    <item>
      <title>Open drain output pin on KL25Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Open-drain-output-pin-on-KL25Z/m-p/230817#M4967</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How should I do to set a GPIO output pin as open drain?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There seems to be no option for that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or should I set the GPIO as input when I want to set the pin high and set the GPIO as low output when I want to set the pin low?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2013 13:56:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Open-drain-output-pin-on-KL25Z/m-p/230817#M4967</guid>
      <dc:creator>markosiponen</dc:creator>
      <dc:date>2013-06-20T13:56:26Z</dc:date>
    </item>
    <item>
      <title>Re: Open drain output pin on KL25Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Open-drain-output-pin-on-KL25Z/m-p/230818#M4968</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Markosiponen&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First, KL series has not open drain control register.&lt;/P&gt;&lt;P&gt;Then I think your solution is OK.&amp;nbsp; One reminder is attention to pull-up resistor value selection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 01:22:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Open-drain-output-pin-on-KL25Z/m-p/230818#M4968</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2013-06-21T01:22:12Z</dc:date>
    </item>
  </channel>
</rss>