<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Couldn't return to main() infinite loop after an ISR responding to an external interrupt is processed in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Couldn-t-return-to-main-infinite-loop-after-an-ISR-responding-to/m-p/820477#M49645</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So, actually, you don't have the debugger, you just use the UART4 to printf the information to following code execuction flow?&lt;/P&gt;&lt;P&gt;It seems your code still blocked anywhere, you can send me your test project, I will help you to check it on my K60D100.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Sep 2018 08:34:31 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2018-09-18T08:34:31Z</dc:date>
    <item>
      <title>Couldn't return to main() infinite loop after an ISR responding to an external interrupt is processed</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Couldn-t-return-to-main-infinite-loop-after-an-ISR-responding-to/m-p/820474#M49642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;Kinetis K50 to collect data from several sensors periodically. I also calibrate the sensor analog circuit upon pushbutton interrupt on Port D. The calibration takes about 30 seconds by adjusting a digital pot controlled by the MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the infinite while loop in main(), a portion of the data is collected through UART interface because the sensor circuit sends out digital reading periodically via UART which create a software interrupt when the&amp;nbsp;data is ready.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Before I pushed the calibration button, everything worked well. However, when I pushed the button and the program went through the calibration ISR for another sensor, the data collection cannot be resumed (It actually only resumed once in one of the experiments, and then never again. The interrupt settings for the pushbutton and UART were exactly the same for both scenarios)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;During debugging, I sent a string to my computer COM port at the end of&amp;nbsp;my ISR, and confirmed the program has run to the end of the ISR. But the data collection in the infinite loop of main() could not be resumed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Couldn't figure out what's the problem, would appreciate it very much if anyone could advise.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following lists the ISR of the pushbutton interrupt and the UART interrupt setting&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void PORTD_IRQHandler(){&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;DisableInterrupts //in header file, I have&amp;nbsp; &amp;nbsp;#define DisableInterrupts asm(" CPSID i");&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;PIT_StopTimer(PIT, kPIT_Chnl_0);&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;packetStart = false;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;if ((PORTD-&amp;gt;ISFR &amp;amp; D_O2_CAL_BUTTON) != 0U){&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;PORTD-&amp;gt;ISFR |= D_O2_CAL_BUTTON; //clear interrupt flag&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;oxyCal(baroPres, stpdFact); //The calibration function&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;}&lt;BR /&gt; PIT_StartTimer(PIT, kPIT_Chnl_0);&lt;BR /&gt; EnableInterrupts&amp;nbsp; //in header file, I have #define EnableInterrupts asm(" CPSIE i");&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void uartInterruptSetup(){&lt;BR /&gt; {&lt;/P&gt;&lt;P&gt;/*Enable Interrupts on UART 0*/&lt;BR /&gt; UART_EnableInterrupts (UART0, kUART_RxDataRegFullInterruptEnable | kUART_RxOverrunInterruptEnable);&lt;BR /&gt; EnableIRQ(UART0_RX_TX_IRQn);&lt;BR /&gt; }&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Sep 2018 19:29:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Couldn-t-return-to-main-infinite-loop-after-an-ISR-responding-to/m-p/820474#M49642</guid>
      <dc:creator>yinni</dc:creator>
      <dc:date>2018-09-12T19:29:33Z</dc:date>
    </item>
    <item>
      <title>Re: Couldn't return to main() infinite loop after an ISR responding to an external interrupt is processed</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Couldn-t-return-to-main-infinite-loop-after-an-ISR-responding-to/m-p/820475#M49643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yinni Cao,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1. Please tell me your K50 full name, because K50 have 72M and 100Mhz chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2. Please set the interrupt priority for port interrupt and the UART interrupt.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 3. Please also share me your main while(1) code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; You said: the data collection in the infinite loop of main() could not be resumed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; So, I need to check your code, please also tell me, after exit the PORTD interrupt, if it can be resumed, where the code is stopping now?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can give me some picture about your debug screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Sep 2018 06:22:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Couldn-t-return-to-main-infinite-loop-after-an-ISR-responding-to/m-p/820475#M49643</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-09-13T06:22:50Z</dc:date>
    </item>
    <item>
      <title>Re: Couldn't return to main() infinite loop after an ISR responding to an external interrupt is processed</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Couldn-t-return-to-main-infinite-loop-after-an-ISR-responding-to/m-p/820476#M49644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there some kind of deadlock going on because of trying to use the UART IRQ from in the other IRQ?&lt;BR /&gt;Problems like this will give a random appearance, such as your 'work once'.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Sep 2018 12:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Couldn-t-return-to-main-infinite-loop-after-an-ISR-responding-to/m-p/820476#M49644</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2018-09-13T12:19:09Z</dc:date>
    </item>
    <item>
      <title>Re: Couldn't return to main() infinite loop after an ISR responding to an external interrupt is processed</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Couldn-t-return-to-main-infinite-loop-after-an-ISR-responding-to/m-p/820477#M49645</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So, actually, you don't have the debugger, you just use the UART4 to printf the information to following code execuction flow?&lt;/P&gt;&lt;P&gt;It seems your code still blocked anywhere, you can send me your test project, I will help you to check it on my K60D100.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Sep 2018 08:34:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Couldn-t-return-to-main-infinite-loop-after-an-ISR-responding-to/m-p/820477#M49645</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-09-18T08:34:31Z</dc:date>
    </item>
  </channel>
</rss>