<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Kinetis K65 Running code from external SDRAM / Flash</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K65-Running-code-from-external-SDRAM-Flash/m-p/819740#M49611</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the later reply.&lt;/P&gt;&lt;P&gt;Customer can run the code from external SDRAM or Flash memory device.&lt;/P&gt;&lt;P&gt;K65 with the cache to access the external SDRAM or Flash memory device, which will enhance the code execute performance.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Aug 2018 02:09:05 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2018-08-07T02:09:05Z</dc:date>
    <item>
      <title>Kinetis K65 Running code from external SDRAM / Flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K65-Running-code-from-external-SDRAM-Flash/m-p/819739#M49610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've been looking at using K65 for a project we have. The software people are not happy with the amount of RAM/NVRAM available so one way or another I have to expand it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it actually possible to run code from SDRAM and/or Flash? And if it is, is the external memory controller smart enough to at least combine two word reads for long instruction into a single read operation instead of doing the whole thing from Activate to Precharge for each word?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In ideal world the K65 would do prefetch and caching i.e. Flash chip initial access may be 90ns but then you can read the rest of the bank at 15ns/pop. This is even more pressing matter for SDRAM which is very burst-oriented technology.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess Kinetis doesn't do that sofisticated memory management thought. i.MX 7 would..&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Aug 2018 15:32:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K65-Running-code-from-external-SDRAM-Flash/m-p/819739#M49610</guid>
      <dc:creator>olli_mannisto</dc:creator>
      <dc:date>2018-08-03T15:32:20Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K65 Running code from external SDRAM / Flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K65-Running-code-from-external-SDRAM-Flash/m-p/819740#M49611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the later reply.&lt;/P&gt;&lt;P&gt;Customer can run the code from external SDRAM or Flash memory device.&lt;/P&gt;&lt;P&gt;K65 with the cache to access the external SDRAM or Flash memory device, which will enhance the code execute performance.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Aug 2018 02:09:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K65-Running-code-from-external-SDRAM-Flash/m-p/819740#M49611</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2018-08-07T02:09:05Z</dc:date>
    </item>
  </channel>
</rss>