<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Meet some problem to make a complementary pwm wave.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Meet-some-problem-to-make-a-complementary-pwm-wave/m-p/819304#M49589</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to make a complementary pwm wave with the code below, but it doesn't work anyway. Is there anything wrong with my code? Using KEA128 and S32DS. Project attached. Please help.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65600i1361A4666D1A4AEC/image-size/large?v=v2&amp;amp;px=999" title="pwm.PNG" alt="pwm.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jul 2018 02:15:27 GMT</pubDate>
    <dc:creator>ayanosun</dc:creator>
    <dc:date>2018-07-17T02:15:27Z</dc:date>
    <item>
      <title>Meet some problem to make a complementary pwm wave.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Meet-some-problem-to-make-a-complementary-pwm-wave/m-p/819304#M49589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to make a complementary pwm wave with the code below, but it doesn't work anyway. Is there anything wrong with my code? Using KEA128 and S32DS. Project attached. Please help.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65600i1361A4666D1A4AEC/image-size/large?v=v2&amp;amp;px=999" title="pwm.PNG" alt="pwm.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 02:15:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Meet-some-problem-to-make-a-complementary-pwm-wave/m-p/819304#M49589</guid>
      <dc:creator>ayanosun</dc:creator>
      <dc:date>2018-07-17T02:15:27Z</dc:date>
    </item>
    <item>
      <title>Re: Meet some problem to make a complementary pwm wave.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Meet-some-problem-to-make-a-complementary-pwm-wave/m-p/819305#M49590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please modify the code shown below:&lt;/P&gt;&lt;P&gt;add PWMPol for FTM2_CH1&lt;/P&gt;&lt;P&gt;Do not recommand to use same CnV for two channel&lt;/P&gt;&lt;P&gt;Select PTH0 and PTH1 as the output pins for these two FTM2 channel.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65840iB0CA8475B96717D5/image-size/large?v=v2&amp;amp;px=999" title="complementary.png" alt="complementary.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have also attached the FRDM_KEA128_FTM_Combine.c file, so that you can direct test it on FRDM-KEA128 board.(...\FRDM-KEA-QSP(REV 8)\Quick Start Package v8\Code Project Examples and Sample Drivers (Evaluation Grade Only)\FRDM-KEAZ128\Driver Test SW for KEAZ128\Driver Test SW for KEAZ128\FRDM_KEA128_FTM_Combine)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2018 07:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Meet-some-problem-to-make-a-complementary-pwm-wave/m-p/819305#M49590</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2018-07-19T07:05:22Z</dc:date>
    </item>
  </channel>
</rss>