<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Treat FTM output pin as GPIO? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Treat-FTM-output-pin-as-GPIO/m-p/816288#M49476</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to write to the output of an FTM pin on the K64? I have pin A12 set up as MuxAlt4 (i.e. as FTM0_CH1), and am ordinarily using Output Compare to set the pin. However, in certain instances, I would like to manually set the pin to high. Can I treat the pin as a GPIO pin to accomplish this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was hoping I could simply write to the GPIO PDOR register for that particular pin (which is PTC2), but doing so seems to have no effect on the pin output level.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Aug 2018 20:09:29 GMT</pubDate>
    <dc:creator>aberger</dc:creator>
    <dc:date>2018-08-22T20:09:29Z</dc:date>
    <item>
      <title>Treat FTM output pin as GPIO?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Treat-FTM-output-pin-as-GPIO/m-p/816288#M49476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to write to the output of an FTM pin on the K64? I have pin A12 set up as MuxAlt4 (i.e. as FTM0_CH1), and am ordinarily using Output Compare to set the pin. However, in certain instances, I would like to manually set the pin to high. Can I treat the pin as a GPIO pin to accomplish this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was hoping I could simply write to the GPIO PDOR register for that particular pin (which is PTC2), but doing so seems to have no effect on the pin output level.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2018 20:09:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Treat-FTM-output-pin-as-GPIO/m-p/816288#M49476</guid>
      <dc:creator>aberger</dc:creator>
      <dc:date>2018-08-22T20:09:29Z</dc:date>
    </item>
    <item>
      <title>Re: Treat FTM output pin as GPIO?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Treat-FTM-output-pin-as-GPIO/m-p/816289#M49477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please check the Initialization feature:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67259iA92A537876887D95/image-size/large?v=v2&amp;amp;px=999" title="40.4.18 Initialization.png" alt="40.4.18 Initialization.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67167i06FD5EB6F2257AE9/image-size/large?v=v2&amp;amp;px=999" title="FTMx_MODE[INIT].png" alt="FTMx_MODE[INIT].png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67208i3E00102F72353F4E/image-size/large?v=v2&amp;amp;px=999" title="FTMx_OUTINIT.png" alt="FTMx_OUTINIT.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Aug 2018 03:06:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Treat-FTM-output-pin-as-GPIO/m-p/816289#M49477</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2018-08-23T03:06:03Z</dc:date>
    </item>
  </channel>
</rss>