<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKinetis SDK FLASH_ProgramPartition() from fsl_flash.c example code</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-SDK-FLASH-ProgramPartition-from-fsl-flash-c-example-code/m-p/815443#M49441</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do we have any example code to setup the EEPROM on MK10DX128 (or K60) with SDK2.2 &amp;nbsp;and especially how to use "FLASH_ProgramPartition" from fsl_flash.c ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Best Regards, &lt;BR /&gt; Philippe.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Oct 2018 13:17:53 GMT</pubDate>
    <dc:creator>phil74</dc:creator>
    <dc:date>2018-10-01T13:17:53Z</dc:date>
    <item>
      <title>Kinetis SDK FLASH_ProgramPartition() from fsl_flash.c example code</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-SDK-FLASH-ProgramPartition-from-fsl-flash-c-example-code/m-p/815443#M49441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do we have any example code to setup the EEPROM on MK10DX128 (or K60) with SDK2.2 &amp;nbsp;and especially how to use "FLASH_ProgramPartition" from fsl_flash.c ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Best Regards, &lt;BR /&gt; Philippe.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Oct 2018 13:17:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-SDK-FLASH-ProgramPartition-from-fsl-flash-c-example-code/m-p/815443#M49441</guid>
      <dc:creator>phil74</dc:creator>
      <dc:date>2018-10-01T13:17:53Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis SDK FLASH_ProgramPartition() from fsl_flash.c example code</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-SDK-FLASH-ProgramPartition-from-fsl-flash-c-example-code/m-p/815444#M49442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Philippe.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suggest you refer to AN4282, Using the Kinetis Family Enhanced EEPROM Functionality&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN4282.pdf" title="https://www.nxp.com/docs/en/application-note/AN4282.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4282.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;and check the section 3.1 FlexMemory partitioning.&lt;/P&gt;&lt;P&gt;If you want to repartition the EEPROM, it is said&amp;nbsp; you can mass erase the chip FlexNVM, and do the EEPROM partitioning.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2018 04:41:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-SDK-FLASH-ProgramPartition-from-fsl-flash-c-example-code/m-p/815444#M49442</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2018-10-02T04:41:58Z</dc:date>
    </item>
  </channel>
</rss>