<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: FTM Filter for Input Capture not working</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Filter-for-Input-Capture-not-working/m-p/814835#M49413</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Andy,&lt;/P&gt;&lt;P&gt;The minimum pulse cycle time is CHnFVAL[3:0] (× 4 system clocks), assume that the system clock is 120MHz for the K64, the minimum pulse cycle time is 16*[1/(120MHz/4)]=500ns.&lt;/P&gt;&lt;P&gt;You says that the capture signal is 5V logic, if you inputs 3.3V logic capture signal, what is the result?&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_277.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74946iF9C70EDFA4FC2293/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_277.png" alt="pastedImage_277.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Oct 2018 09:38:38 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2018-10-08T09:38:38Z</dc:date>
    <item>
      <title>FTM Filter for Input Capture not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Filter-for-Input-Capture-not-working/m-p/814833#M49411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm sending a 0-5 V square wave signal into FTM1_CH0 of a K64, with the input filter value set to 16, and the mode set to detect rising edges. By my understanding, that means that the&amp;nbsp;FTM requires the input signal to remain in a high state for 16 bus clock cycles (i.e. 260 ns with bus clock = 60 MHz) following a low-to-high transition before it sets the CHnF flag and writes the input capture register C(n)V with the counter value. However, I've discovered that the FTM is occasionally counting small glitches on the input signal as a true edge.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="FTM Glitch Events.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73659i0D35510A7734A053/image-size/large?v=v2&amp;amp;px=999" role="button" title="FTM Glitch Events.png" alt="FTM Glitch Events.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Above is a scope trace showing six true edges and two glitch events that cause false edge triggers. To capture this scope trace, I have caused a GPIO pin to toggle (channel 1, yellow) in the FTM ISR that is fired whenever an edge is detected on the input signal (channel 3, blue).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Zooming in on the glitch events, I see that they do not last the minimum duration set by the input filter value (there is a very brief spike, &amp;lt; 50 ns, on the input signal). Furthermore, the input high level is not &amp;gt; 0.7*V_DD, as required to be considered an input high voltage. (I have V_DD set to 1.8 V, so the input signal needs to be at least 1.26 V. Here it looks like it maybe reaches 800 mV... although perhaps maybe my scope is not resolving the true peak height). Lastly, you can also see that this type of glitch event does not always cause an edge detection event (bottom panel).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="FTM Glitch Events (zoom).png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73698i939375CD063901CB/image-size/large?v=v2&amp;amp;px=999" role="button" title="FTM Glitch Events (zoom).png" alt="FTM Glitch Events (zoom).png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;What would the reason be for this sort of behavior of the FTM input capture filter for edge detection?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Oct 2018 17:51:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Filter-for-Input-Capture-not-working/m-p/814833#M49411</guid>
      <dc:creator>aberger</dc:creator>
      <dc:date>2018-10-01T17:51:23Z</dc:date>
    </item>
    <item>
      <title>Re: FTM Filter for Input Capture not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Filter-for-Input-Capture-not-working/m-p/814834#M49412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figured out the question of signal magnitude: with such a short pulse, the cable I was using to probe the CH3 signal in the above figures was loading down the input signal. By using a scope probe cable instead of a BNC cable, I could see that the signal could very well be rising to the 0.7*V_DD threshold to be considered an input high voltage level.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nevertheless, the issue of FTM Input Filtering remains. The pulse duration is less than 16 times the FTM source clock, so I still believe that this short pulse should&amp;nbsp;&lt;EM&gt;not&lt;/EM&gt; be triggering the FTM.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Oct 2018 19:49:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Filter-for-Input-Capture-not-working/m-p/814834#M49412</guid>
      <dc:creator>aberger</dc:creator>
      <dc:date>2018-10-03T19:49:38Z</dc:date>
    </item>
    <item>
      <title>Re: FTM Filter for Input Capture not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Filter-for-Input-Capture-not-working/m-p/814835#M49413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Andy,&lt;/P&gt;&lt;P&gt;The minimum pulse cycle time is CHnFVAL[3:0] (× 4 system clocks), assume that the system clock is 120MHz for the K64, the minimum pulse cycle time is 16*[1/(120MHz/4)]=500ns.&lt;/P&gt;&lt;P&gt;You says that the capture signal is 5V logic, if you inputs 3.3V logic capture signal, what is the result?&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_277.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74946iF9C70EDFA4FC2293/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_277.png" alt="pastedImage_277.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Oct 2018 09:38:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Filter-for-Input-Capture-not-working/m-p/814835#M49413</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-10-08T09:38:38Z</dc:date>
    </item>
    <item>
      <title>Re: FTM Filter for Input Capture not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Filter-for-Input-Capture-not-working/m-p/1857956#M66337</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This hasn't answered the question.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a similar problem:&amp;nbsp;&lt;/P&gt;&lt;P&gt;SystemClk = 120MHz; Pre-scaler = divide by 1&lt;/P&gt;&lt;P&gt;Filter:&lt;/P&gt;&lt;P&gt;The signal to be captured by FTM1 Ch0 is Freq_Mon = 1MHz.&lt;BR /&gt;The signal when present has been verified by oscilloscope.&lt;/P&gt;&lt;P&gt;The minimum pulse width to be passed by the filter is:&lt;/P&gt;&lt;P&gt;1/2 Freq_Mon = 500ns.&lt;BR /&gt;&lt;BR /&gt;From the manual [Ref: P972 K24 Sub-Family Reference Manual, Rev. 2, January 2014]&lt;BR /&gt;it states that:&lt;/P&gt;&lt;P&gt;minimum pulse width = CHnFVAL[3:0] x 4 system clocks&lt;/P&gt;&lt;P&gt;4 system clocks = 1/120MHz x 4&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; = 8.3ns x 4&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; = 33.33ns&lt;/P&gt;&lt;P&gt;so&lt;/P&gt;&lt;P&gt;CHnFVAL[3:0] = 500ns / 33.33ns&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; = 15&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; // Stops capturing. Tried 14 and get same result&lt;/P&gt;&lt;P&gt;However:&lt;/P&gt;&lt;P&gt;Setting CHnFVAL[3:0] = 7 passes a pulse of 500ns&lt;BR /&gt;Setting CHnFVAL[3:0] = 8 stops a pulse of 500ns&lt;/P&gt;&lt;P&gt;This infers the system clock is divided by 2. i.e. 60MHz&lt;/P&gt;&lt;P&gt;e.g.&lt;/P&gt;&lt;P&gt;4 system clocks = 1/60MHz x 4&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; = 16.67ns x 4&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; = 66.67ns&lt;/P&gt;&lt;P&gt;so&lt;/P&gt;&lt;P&gt;CHnFVAL[3:0]&amp;nbsp; &amp;nbsp;= 500ns / 66.67ns&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; = 7.5&amp;nbsp; (7) works fine, but I don't understand why?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Implementation:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;void FTM1_DRV_InputCaptureInit(void)
{
    // Enable clock to the FTM1 module
    SIM_SCGC6 |= SIM_SCGC6_FTM1_MASK;
    
    // Configure pin 64 and its alternate function for FTM1 Ch 0. pin PTA12 (64)    
    PORTA_PCR12 = PORT_PCR_MUX(3);
    
    // Disable write protection for FTM1 registers
    FTM1_MODE |= FTM_MODE_WPDIS_MASK;
    
    // Configure FTM1 as input capture
    FTM1_SC = 0;                        // Ensure FTM1 is disabled for setup
    FTM1_SC &amp;amp;= ~FTM_SC_TOIE_MASK;       // Disable Timer Overflow Interrupt
    FTM1_SC &amp;amp;= ~FTM_SC_TOF_MASK;        // Clear Timer Overflow Event flag
    FTM1_CNTIN = 0;                     // Count reset to 0
    FTM1_MOD = 0xFFFF;                  // Set the modulo register for maximum count

    // The clk source is set to 120MHz by FTM1_DRV_CaptureStart() every 500ms.    
    FTM1_SC &amp;amp;= ~FTM_SC_CLKS(7);         // Select NO clock.
    FTM1_SC |= FTM_SC_PS(0);            // Select prescaler divide by 1.
    
    // Configure FTM1 Channel 0 for input capture on rising edge only
    FTM1_C0SC = FTM_CnSC_ELSA_MASK;     // Capture on rising edge
       
    FTM1_FILTER |= FTM_FILTER_CH0FVAL(7);  // Half the input period
                                           // (120MHz / 4) x FVAL = 500ns 
                                           // FVAL = 500 / 33.33 = 15.
                                           // This value stops the ISR
                                           // (Using 60MHz / 4) x FVAL = 500ns
                                           // FVAL = 500 / 66.67 = 7.5
                                           // Use 7 and runs ok
                                           // Dont know why using the value of
                                           // SYS_CLK doesnt work.
                                           // The frequency set in SC reg is SYS_CLK
                                            
#ifdef DEBUG_CPT
    // Enable CAPTEST mode for FTM1 (simulate input capture events internally)
    FTM1_CONF |= FTM_CONF_CAPTEST_MASK;
#endif

    /* Configure NVIC. Register interrupt into Ram Vector table */
    os_install_int_handler (g_ftmIrqId[HW_FTM1], FTM1_ISR);
    
    NVIC_SetPriority(FTM1_IRQn, 1); // ISR runs every 500ms for ?ns
    
    NVIC_ClearPendingIRQ(g_ftmIrqId[HW_FTM1]);
    
    /* Enable FTM interrupt in NVIC level.*/
    INT_SYS_EnableIRQ(g_ftmIrqId[HW_FTM1]);
    
    // Make sure these are reset at initailization.
    count = 0;
    freq_mon_fault = false;
}&lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 01 May 2024 12:03:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Filter-for-Input-Capture-not-working/m-p/1857956#M66337</guid>
      <dc:creator>DaveTonyCook</dc:creator>
      <dc:date>2024-05-01T12:03:03Z</dc:date>
    </item>
  </channel>
</rss>