<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: USB Packets sniffer unit</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Packets-sniffer-unit/m-p/811871#M49307</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Riccardo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Due to the speed that this may require I'm not sure that a Kinetis MCU is the best option. If you want to use the Kinetis you will need something to deal with the reception of the data, like an FPGA.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Probably the best option is a processor of the i.MX family which are way much faster than the Kinetis MCUs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately, we don't have examples of a USB sniffer for any of the families mentioned before.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Oct 2018 18:06:14 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2018-10-23T18:06:14Z</dc:date>
    <item>
      <title>USB Packets sniffer unit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Packets-sniffer-unit/m-p/811870#M49306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Good morning I am searching for a solution to implement an USB Sniffer unit.&lt;BR /&gt;I need to connect to a standard Host - Device USB connection with a 3rd unit (The Sniffer) that without influencing the original Host-Device link it will be capable to read and interpret the USB data flow of the original link.&lt;BR /&gt;It shall be a kind of USB data protocol analyzer.&lt;BR /&gt;Do you know an Hardware/Software solution (either MCU or MPU ) and example implementing this function ?&lt;P&gt;&lt;/P&gt;Many thanks Paccciani Riccardo&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Sep 2018 04:42:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Packets-sniffer-unit/m-p/811870#M49306</guid>
      <dc:creator>jp66riccardo</dc:creator>
      <dc:date>2018-09-30T04:42:53Z</dc:date>
    </item>
    <item>
      <title>Re: USB Packets sniffer unit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Packets-sniffer-unit/m-p/811871#M49307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Riccardo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Due to the speed that this may require I'm not sure that a Kinetis MCU is the best option. If you want to use the Kinetis you will need something to deal with the reception of the data, like an FPGA.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Probably the best option is a processor of the i.MX family which are way much faster than the Kinetis MCUs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately, we don't have examples of a USB sniffer for any of the families mentioned before.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2018 18:06:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Packets-sniffer-unit/m-p/811871#M49307</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-10-23T18:06:14Z</dc:date>
    </item>
  </channel>
</rss>