<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: kl16 dma with enable circular</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl16-dma-with-enable-circular/m-p/811438#M49301</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ensure that the memory that you are receiving the data to is also modulo aligned. That is, if you use modulo 16 make sure that it starts on a boundary that is divisible by 16; eg. 0x20000000, 0x20000010, 0x20000020, etc. when in SRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Dec 2018 21:46:55 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2018-12-18T21:46:55Z</dc:date>
    <item>
      <title>kl16 dma with enable circular</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl16-dma-with-enable-circular/m-p/811437#M49300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I use KL16&amp;nbsp; DMA&amp;nbsp; for uart transfer .&lt;/P&gt;&lt;P&gt;When i use DMA, i enable&amp;nbsp; DMOD (Destination Address Modulo) ，and set circular buffer size 16 bytes(DMOD writed 0000) ，.&lt;/P&gt;&lt;P&gt;After&amp;nbsp; uart&amp;nbsp; trans&amp;nbsp; 16&amp;nbsp; bytes,&amp;nbsp; receive_buffer will&amp;nbsp; lost the last data(receive_buffer[15]), and&amp;nbsp; BCR value&amp;nbsp; is right.&lt;/P&gt;&lt;P&gt;The same&amp;nbsp; thing happens when DMOD be set to 0010.Will lost receive_buffer[31].&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70116iD2DCBDC152568A45/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70146i8640811751AE81B3/image-size/large?v=v2&amp;amp;px=999" title="2.png" alt="2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Dec 2018 12:15:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl16-dma-with-enable-circular/m-p/811437#M49300</guid>
      <dc:creator>yourchoochoo</dc:creator>
      <dc:date>2018-12-18T12:15:08Z</dc:date>
    </item>
    <item>
      <title>Re: kl16 dma with enable circular</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl16-dma-with-enable-circular/m-p/811438#M49301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ensure that the memory that you are receiving the data to is also modulo aligned. That is, if you use modulo 16 make sure that it starts on a boundary that is divisible by 16; eg. 0x20000000, 0x20000010, 0x20000020, etc. when in SRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Dec 2018 21:46:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl16-dma-with-enable-circular/m-p/811438#M49301</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-12-18T21:46:55Z</dc:date>
    </item>
  </channel>
</rss>