<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 K65P169M180SF5V2 GPIO Voltage Limits on Startup</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65P169M180SF5V2-GPIO-Voltage-Limits-on-Startup/m-p/811409#M49297</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is a question about the voltage limits of the K65P169M180SF5V2 GPIOs during startup.&lt;/P&gt;&lt;P&gt;Assuming that we have a peripheral powered with +5V and the K65 powered by an +3V3 LDO connected to this same +5V.&lt;/P&gt;&lt;P&gt;This periheral has a TX line connected via a voltage divider to an K65 GPIO that limits the input voltages to a safe level (max. ~3,3V).&lt;/P&gt;&lt;P&gt;In this situation the +5V can be present earlier at the voltage divider than the +3V3 supply at the K65, i.e. at startup the input voltage can be higher than the in datasheet specified VDIO_MAX&amp;nbsp; of VDD+0.3V.&lt;/P&gt;&lt;P&gt;Other posts (&lt;A href="https://community.nxp.com/thread/433880"&gt;https://community.nxp.com/thread/433880&lt;/A&gt; ) clarify that the K-Series does not have protection diodes to VDD.&lt;/P&gt;&lt;P&gt;Therefore I assume, that in this situation the K65 works outside the safe specification and can be damaged, even if the series resistor of the voltage divider limits the current (e.g. &amp;lt;1mA).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this view correct or can the K65 tolerate such transient events?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;B.Hofer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Nov 2018 14:01:55 GMT</pubDate>
    <dc:creator>bhofer</dc:creator>
    <dc:date>2018-11-07T14:01:55Z</dc:date>
    <item>
      <title>K65P169M180SF5V2 GPIO Voltage Limits on Startup</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65P169M180SF5V2-GPIO-Voltage-Limits-on-Startup/m-p/811409#M49297</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is a question about the voltage limits of the K65P169M180SF5V2 GPIOs during startup.&lt;/P&gt;&lt;P&gt;Assuming that we have a peripheral powered with +5V and the K65 powered by an +3V3 LDO connected to this same +5V.&lt;/P&gt;&lt;P&gt;This periheral has a TX line connected via a voltage divider to an K65 GPIO that limits the input voltages to a safe level (max. ~3,3V).&lt;/P&gt;&lt;P&gt;In this situation the +5V can be present earlier at the voltage divider than the +3V3 supply at the K65, i.e. at startup the input voltage can be higher than the in datasheet specified VDIO_MAX&amp;nbsp; of VDD+0.3V.&lt;/P&gt;&lt;P&gt;Other posts (&lt;A href="https://community.nxp.com/thread/433880"&gt;https://community.nxp.com/thread/433880&lt;/A&gt; ) clarify that the K-Series does not have protection diodes to VDD.&lt;/P&gt;&lt;P&gt;Therefore I assume, that in this situation the K65 works outside the safe specification and can be damaged, even if the series resistor of the voltage divider limits the current (e.g. &amp;lt;1mA).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this view correct or can the K65 tolerate such transient events?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;B.Hofer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Nov 2018 14:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65P169M180SF5V2-GPIO-Voltage-Limits-on-Startup/m-p/811409#M49297</guid>
      <dc:creator>bhofer</dc:creator>
      <dc:date>2018-11-07T14:01:55Z</dc:date>
    </item>
    <item>
      <title>Re: K65P169M180SF5V2 GPIO Voltage Limits on Startup</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65P169M180SF5V2-GPIO-Voltage-Limits-on-Startup/m-p/811410#M49298</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are correct that K65 can not "safe" working as the situation you mentioned. Even though this startup duration is short, we really do not recommend used as this case.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Nov 2018 16:17:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65P169M180SF5V2-GPIO-Voltage-Limits-on-Startup/m-p/811410#M49298</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2018-11-08T16:17:28Z</dc:date>
    </item>
    <item>
      <title>Re: K65P169M180SF5V2 GPIO Voltage Limits on Startup</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65P169M180SF5V2-GPIO-Voltage-Limits-on-Startup/m-p/811411#M49299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the answer! So since this applies also to all analog pins, standard applications such as monitoring the device supply voltage (e.g. +5V or +12V over a voltage divider) face the same situation and require an external protection measure (e.g. diode to VDD and current limiting resistzor).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why is this not clearly stated in the datasheet and instead hidden in some footnote?!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Nov 2018 14:53:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65P169M180SF5V2-GPIO-Voltage-Limits-on-Startup/m-p/811411#M49299</guid>
      <dc:creator>bhofer</dc:creator>
      <dc:date>2018-11-12T14:53:33Z</dc:date>
    </item>
  </channel>
</rss>