<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K81 execution fails with UART attached in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808536#M49154</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Denis Collis,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Thank you for your updated information.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I don't think the pull up in the UART pin is the key point, but the TTL-USB really influence your MCU work.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Now, please check these points.&lt;/P&gt;&lt;P&gt;1. Please add the LED blinking or the GPIO toggle code, just check when your UART can't work, whether your other code, eg, LED blinky can work?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Just make sure whether the code is stopped anywhere.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Please modify your FOPT, the flash address is 0x40d, you can change the code boot from the internal flash directly, instead of boot from the ROM after rest.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/68662i4083E8BE8A59C6B7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Then download your code again.&lt;/P&gt;&lt;P&gt;Check whether the problem still happens or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. When you connect the TTL-USB, please add the GND connect to your board GND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4. Please also use the oscilloscope to check your NMI pin during the reset. Whether it has the pull low problem or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please try it again.&lt;/P&gt;&lt;P&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Sep 2018 05:35:59 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2018-09-13T05:35:59Z</dc:date>
    <item>
      <title>K81 execution fails with UART attached</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808532#M49150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My K81 project firmware communicates to&amp;nbsp;a PC-hosted application via LPUART2&amp;nbsp;through an FTDI USB-to-Serial_TTL cable.&lt;/P&gt;&lt;P&gt;If I&amp;nbsp;run in debug&amp;nbsp;- i.e. Segger J-Link attached and under control of MCUXpresso's debug environment - with or without the serial cable attached, then everything works.&lt;/P&gt;&lt;P&gt;If I reset the K81 board with the serial cable DETACHED, &lt;SPAN&gt;then everything works.&amp;nbsp; If I attach the serial cable while the board is running, then everything continues to work.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;But...&amp;nbsp; &amp;nbsp;...If I reset the K81 board with the serial cable ATTACHED, the K81 is usually unresponsive, but occasionally works.&lt;/P&gt;&lt;P&gt;Note: No semi-hosting (using&amp;nbsp;libcr_nohost_nf.a)&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas on how to track and solve this problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Sep 2018 22:36:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808532#M49150</guid>
      <dc:creator>deniscollis</dc:creator>
      <dc:date>2018-09-10T22:36:22Z</dc:date>
    </item>
    <item>
      <title>Re: K81 execution fails with UART attached</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808533#M49151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The 'occasionally works' is now deterministic.&amp;nbsp; I've discovered that:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;The board always runs if reset immediately after connecting the serial cable&lt;/LI&gt;&lt;LI&gt;The board always fails if reset without disconnecting and reconnecting the serial cable.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;So, there appears to be something coming from the PC serial port that is destabilizing the LPUART.&amp;nbsp; &amp;nbsp;I also noticed in the circuit schematic that there are no external pull-up resistors on the board.&amp;nbsp; There aren't any in the USB-to-Serial cable either.&amp;nbsp; I manually patched the board by adding a pair of weak 470K pull-ups to the TX and RX lines.&amp;nbsp; That did not help at all: I probably need something a bit stronger, say, 70K-100K?&lt;/P&gt;&lt;P&gt;I have no idea why the problem does not manifest in debug mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Sep 2018 23:53:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808533#M49151</guid>
      <dc:creator>deniscollis</dc:creator>
      <dc:date>2018-09-11T23:53:05Z</dc:date>
    </item>
    <item>
      <title>Re: K81 execution fails with UART attached</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808534#M49152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Denis Collis,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please add the 4.7K to 10K pull up in your NMI pin, then try it again.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; From your description, it seems your chip enter the ROM bootloader mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; So, make sure when your reset the chip, the NMI pin is high.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;----------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Sep 2018 03:01:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808534#M49152</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-09-12T03:01:29Z</dc:date>
    </item>
    <item>
      <title>Re: K81 execution fails with UART attached</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808535#M49153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I meant that there are no external pull-up resistors on the LPUART pins on the board.&amp;nbsp; As you can see, the 10K pull-up on NMI is designed in, so I do not think we have entered ROM bootloader mode.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="NMI_pullup.jpg"&gt;&lt;IMG alt="NMI_pullup.jpg" src="https://community.nxp.com/t5/image/serverpage/image-id/68701iAC4F5FCB394A5866/image-size/large?v=v2&amp;amp;px=999" title="NMI_pullup.jpg" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Theory:&lt;BR /&gt;There is an immediate bus hard-fault when the MCU starts, most likely because&amp;nbsp;K81 POR takes place before the hardware (power and comms) is fully stable.&amp;nbsp; In the debug environment the MCU is reset within fully stable hardware, and so the problem does not manifest.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To test theory:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Connect temporary MCU reset button. (currently this is stabilized with a 4.7K pull-up and 0.001uF to GND)&lt;BR /&gt;-AND- / -OR-&lt;/LI&gt;&lt;LI&gt;Modify HardFault_Handler() to force a system reset after a short delay.&lt;BR /&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"core_cm4.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;__asm&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="string token"&gt;"nop"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;__asm&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="string token"&gt;"nop"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;__asm&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="string token"&gt;"nop"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;__asm&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="string token"&gt;"nop"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;__NVIC_SystemReset&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the interim I have a procedural solution for the user:&amp;nbsp; "The device should be powered up before inserting the USB-to-serial cable into the PC host."&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 14:11:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808535#M49153</guid>
      <dc:creator>deniscollis</dc:creator>
      <dc:date>2020-11-02T14:11:47Z</dc:date>
    </item>
    <item>
      <title>Re: K81 execution fails with UART attached</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808536#M49154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Denis Collis,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Thank you for your updated information.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I don't think the pull up in the UART pin is the key point, but the TTL-USB really influence your MCU work.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Now, please check these points.&lt;/P&gt;&lt;P&gt;1. Please add the LED blinking or the GPIO toggle code, just check when your UART can't work, whether your other code, eg, LED blinky can work?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Just make sure whether the code is stopped anywhere.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Please modify your FOPT, the flash address is 0x40d, you can change the code boot from the internal flash directly, instead of boot from the ROM after rest.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/68662i4083E8BE8A59C6B7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Then download your code again.&lt;/P&gt;&lt;P&gt;Check whether the problem still happens or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. When you connect the TTL-USB, please add the GND connect to your board GND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4. Please also use the oscilloscope to check your NMI pin during the reset. Whether it has the pull low problem or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please try it again.&lt;/P&gt;&lt;P&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Sep 2018 05:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808536#M49154</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-09-13T05:35:59Z</dc:date>
    </item>
    <item>
      <title>Re: K81 execution fails with UART attached</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808537#M49155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Serial data on particular UARTS can send the part into the bootloader at power up.&lt;BR /&gt;See&amp;nbsp;enabledPeripherals in the bootloader BCA in the bootloader manual.&lt;/P&gt;&lt;P&gt;I've run into this in the past myself. :-(&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Sep 2018 12:34:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808537#M49155</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2018-09-13T12:34:41Z</dc:date>
    </item>
    <item>
      <title>Re: K81 execution fails with UART attached</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808538#M49156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Everything looks normal, except a slightly noisy power-up:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;OK: LED blinker working&lt;/LI&gt;&lt;LI&gt;OK: BOOTSRC_SEL is 0&lt;/LI&gt;&lt;LI&gt;OK: TTL_USB GND connected to board GND&lt;/LI&gt;&lt;LI&gt;OK: Scope shows NMI is stable high,&amp;nbsp;with about 100μs transitioning ramp from 0V to 3.3V.&amp;nbsp; However, the first 50&lt;SPAN&gt;μs of the ramp is a bit noisy.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There's no need for me to&amp;nbsp;pursue this any further.&amp;nbsp;&amp;nbsp;I am satisfied that I now understand how the system behaves, and this is sufficient for my immediate development needs.&amp;nbsp;&amp;nbsp;The final production version will not have a serial connection to the PC (that's for the Device Test Environment only), the K81's power will be controlled by a supervisor MCU, and the entire system will be battery powered. I expect the production behavior to be stable and predictable.&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help, and best regards,&lt;/P&gt;&lt;P&gt;Denis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Sep 2018 16:30:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808538#M49156</guid>
      <dc:creator>deniscollis</dc:creator>
      <dc:date>2018-09-13T16:30:22Z</dc:date>
    </item>
    <item>
      <title>Re: K81 execution fails with UART attached</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808539#M49157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Denis,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks a lot for your updated information.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; So, do you mean the LED blinker working, just the TTL-USB? If yes, I suggest you also add the oscilloscope to check the UART TX pin, if the have the wave, the problem may in your TTL-USB tool side, not the MCU side. Because your MCU is still working, not blocked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Sep 2018 06:41:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808539#M49157</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-09-14T06:41:17Z</dc:date>
    </item>
    <item>
      <title>Re: K81 execution fails with UART attached</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808540#M49158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I meant is that the LED mechanism is working - it blinks when the system runs, and does not blink when the system fails.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Denis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Sep 2018 21:35:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808540#M49158</guid>
      <dc:creator>deniscollis</dc:creator>
      <dc:date>2018-09-20T21:35:16Z</dc:date>
    </item>
    <item>
      <title>Re: K81 execution fails with UART attached</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808541#M49159</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Denis,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You said, your reset pin have 4.7K pull up and 0.001uF&amp;nbsp; capacitor to ground, is it right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If yes, please check the 0.001uF&amp;nbsp; capacitor to 0.1uF capacitor, then remove the debugger from the JTAG interface and try it again. 0.001uF&amp;nbsp; is too small.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Sep 2018 05:47:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-execution-fails-with-UART-attached/m-p/808541#M49159</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-09-21T05:47:39Z</dc:date>
    </item>
  </channel>
</rss>