<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Do I need to pull-up RESET_b pin in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-I-need-to-pull-up-RESET-b-pin/m-p/230453#M4915</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;I don't think it's necessary to pull up Reset pin after disable it. Could you tell me whether you had check the RCM_SRSn registers? If not, I suggest you'd better to check the RCM_SRSn registers after reset happens to figure out the source which cause MCU reset. &lt;/P&gt;&lt;P&gt;I'm looking forward to your reply.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 12 Jan 2014 10:37:26 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2014-01-12T10:37:26Z</dc:date>
    <item>
      <title>Do I need to pull-up RESET_b pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-I-need-to-pull-up-RESET-b-pin/m-p/230452#M4914</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; even though I disable it in my chip configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My design is not stable, resets under some situations, seems like a hardware issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindest Regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Jan 2014 07:16:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-I-need-to-pull-up-RESET-b-pin/m-p/230452#M4914</guid>
      <dc:creator>lokuate</dc:creator>
      <dc:date>2014-01-12T07:16:46Z</dc:date>
    </item>
    <item>
      <title>Re: Do I need to pull-up RESET_b pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-I-need-to-pull-up-RESET-b-pin/m-p/230453#M4915</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;I don't think it's necessary to pull up Reset pin after disable it. Could you tell me whether you had check the RCM_SRSn registers? If not, I suggest you'd better to check the RCM_SRSn registers after reset happens to figure out the source which cause MCU reset. &lt;/P&gt;&lt;P&gt;I'm looking forward to your reply.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Jan 2014 10:37:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-I-need-to-pull-up-RESET-b-pin/m-p/230453#M4915</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2014-01-12T10:37:26Z</dc:date>
    </item>
    <item>
      <title>Re: Do I need to pull-up RESET_b pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-I-need-to-pull-up-RESET-b-pin/m-p/230454#M4916</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For hardware design, it is better to add pull-up resistor to reset pin. As you know, there is a internal pull-up resistor in our MCU, but it is only a weak pull-up. So it is recommend to add external one. If your software can run well most time, only will cause reset sometime by unstable reset signal. I think it might cause by non-external pull-up resistor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2014 01:16:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-I-need-to-pull-up-RESET-b-pin/m-p/230454#M4916</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2014-01-13T01:16:42Z</dc:date>
    </item>
  </channel>
</rss>