<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: K22 Not Communicating</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-Communicating/m-p/807906#M49103</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is a custom board, but it doesn't communicate through the SWD connector, both JLink and SWD work. I'm wondering if the chip is faulty or if it a board connection. I have a few other produced boards that do work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Jul 2018 15:42:49 GMT</pubDate>
    <dc:creator>burgeh</dc:creator>
    <dc:date>2018-07-16T15:42:49Z</dc:date>
    <item>
      <title>K22 Not Communicating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-Communicating/m-p/807904#M49101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was brought a K22FN256LH12 board that I just got back from production, and when I plug the J-Link Pro in it instantly turns the LED red. I am also unable to communicate using the JLink commander. Below are images of the errors I keep getting. It says the protection bit is enabled it seems, and therefore I allow it to do a mass erase, but then it still cannot communicate with the board. Any thoughts or is this board shot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65463i5B3EB8C225D3EE26/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65464i6F3ACB728B00666B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2018 14:49:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-Communicating/m-p/807904#M49101</guid>
      <dc:creator>burgeh</dc:creator>
      <dc:date>2018-07-12T14:49:24Z</dc:date>
    </item>
    <item>
      <title>Re: K22 Not Communicating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-Communicating/m-p/807905#M49102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Christopher,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; What's the K22 board you are using now? FRDM-K22?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If yes, please choose the SWD instead of the JTAG, because this board is using the SWD, not the JTAG.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65482i2FB9EE88C3709A32/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jul 2018 05:22:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-Communicating/m-p/807905#M49102</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-07-13T05:22:02Z</dc:date>
    </item>
    <item>
      <title>Re: K22 Not Communicating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-Communicating/m-p/807906#M49103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is a custom board, but it doesn't communicate through the SWD connector, both JLink and SWD work. I'm wondering if the chip is faulty or if it a board connection. I have a few other produced boards that do work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jul 2018 15:42:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-Communicating/m-p/807906#M49103</guid>
      <dc:creator>burgeh</dc:creator>
      <dc:date>2018-07-16T15:42:49Z</dc:date>
    </item>
    <item>
      <title>Re: K22 Not Communicating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-Communicating/m-p/807907#M49104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Christopher,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Now, what's the problem in the custom board? Secure?&lt;/P&gt;&lt;P&gt;&amp;nbsp; If yes, please let our customer check this post:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/servlet/JiveServlet/download/857127-1-396709/Kinetis Lock issue analysis and unlock way.pdf" title="https://community.nxp.com/servlet/JiveServlet/download/857127-1-396709/Kinetis%20Lock%20issue%20analysis%20and%20unlock%20way.pdf"&gt;https://community.nxp.com/servlet/JiveServlet/download/857127-1-396709/Kinetis%20Lock%20issue%20analysis%20and%20unlock%…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This should be the customer board's hardware problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 09:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-Communicating/m-p/807907#M49104</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-07-18T09:25:32Z</dc:date>
    </item>
  </channel>
</rss>