<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックJump to two different application in QSPI using freedom_bootloader</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Jump-to-two-different-application-in-QSPI-using-freedom/m-p/805362#M48955</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using FRDMK82F board. I have two different version of firmware(V1 &amp;amp; V2). V1 will be placed at QSPI&amp;nbsp;0x68001000 and V2 will be placed at QSPI &lt;SPAN&gt;0x68005000&amp;nbsp;&lt;/SPAN&gt;. Internal flash memory flag (01 - V1 and 02 - V2) decides the target user app version V1 or V2. Based on the flag, freedom boot loader should jump to QSPI user application V1 or V2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have done the configuration in freedom_bootloader version K2.0.0 (refer the attached screenshot)&lt;/P&gt;&lt;P&gt;1. get_user_application_entry&lt;/P&gt;&lt;P&gt;2. bootloader_config.h&lt;/P&gt;&lt;P&gt;3. vector_table_info.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then i have configured the QSPI and transferred application .srec with QSPI addrss&amp;nbsp;&lt;SPAN&gt;0x68005000(linker file change and QSPI config logs attached). Application is not booting.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have already booted the same bubble from QSPI @ 0x68001000 using ROM bootloader(K1.3.0).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have done the same user application jump in internal memory for address 0xA000 and 0x10000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;R.Dhanapal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Sep 2018 13:06:49 GMT</pubDate>
    <dc:creator>dhanapal_rajend</dc:creator>
    <dc:date>2018-09-27T13:06:49Z</dc:date>
    <item>
      <title>Jump to two different application in QSPI using freedom_bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Jump-to-two-different-application-in-QSPI-using-freedom/m-p/805362#M48955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using FRDMK82F board. I have two different version of firmware(V1 &amp;amp; V2). V1 will be placed at QSPI&amp;nbsp;0x68001000 and V2 will be placed at QSPI &lt;SPAN&gt;0x68005000&amp;nbsp;&lt;/SPAN&gt;. Internal flash memory flag (01 - V1 and 02 - V2) decides the target user app version V1 or V2. Based on the flag, freedom boot loader should jump to QSPI user application V1 or V2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have done the configuration in freedom_bootloader version K2.0.0 (refer the attached screenshot)&lt;/P&gt;&lt;P&gt;1. get_user_application_entry&lt;/P&gt;&lt;P&gt;2. bootloader_config.h&lt;/P&gt;&lt;P&gt;3. vector_table_info.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then i have configured the QSPI and transferred application .srec with QSPI addrss&amp;nbsp;&lt;SPAN&gt;0x68005000(linker file change and QSPI config logs attached). Application is not booting.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have already booted the same bubble from QSPI @ 0x68001000 using ROM bootloader(K1.3.0).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have done the same user application jump in internal memory for address 0xA000 and 0x10000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;R.Dhanapal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2018 13:06:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Jump-to-two-different-application-in-QSPI-using-freedom/m-p/805362#M48955</guid>
      <dc:creator>dhanapal_rajend</dc:creator>
      <dc:date>2018-09-27T13:06:49Z</dc:date>
    </item>
    <item>
      <title>Re: Jump to two different application in QSPI using freedom_bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Jump-to-two-different-application-in-QSPI-using-freedom/m-p/805363#M48956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dhanapal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting with debug of freedom_bootloader, can you try to jump in to&amp;nbsp;application (add debugging application together with freedom_bootloader) entry point and find what issue you get?&amp;nbsp;Can you share snapshots(call stack, disassembly, register dump etc) of the issue with debugger?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Biswanath&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Oct 2018 04:18:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Jump-to-two-different-application-in-QSPI-using-freedom/m-p/805363#M48956</guid>
      <dc:creator>biswanath_bhowmick</dc:creator>
      <dc:date>2018-10-01T04:18:34Z</dc:date>
    </item>
  </channel>
</rss>