<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: AN2295 Serial Bootloader &amp;quot;SlaveFrequencyCalibration()&amp;quot;</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/AN2295-Serial-Bootloader-quot-SlaveFrequencyCalibration-quot/m-p/230244#M4893</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rabbit,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SlaveFrequencyCalibration() is used to measures break impulse from PC and sets correct trim value, it firstly set UART RX pin as GPIO function and wait for the falling edge on it and then start to count the systick with the help of systick timer till it observes a rising edge on that pin, then it uses the result to calculate the trim value, but as the device doesn't support float point, so the final value might have some offset in some cases.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please kindly let me know if you have any further question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!!&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Feb 2014 06:52:48 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2014-02-18T06:52:48Z</dc:date>
    <item>
      <title>AN2295 Serial Bootloader "SlaveFrequencyCalibration()"</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/AN2295-Serial-Bootloader-quot-SlaveFrequencyCalibration-quot/m-p/230243#M4892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; In AN2295_Kinetis.eww, does anyone know how this function "SlaveFrequencyCalibration()" works? It doesn't work reliable.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2014 07:00:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/AN2295-Serial-Bootloader-quot-SlaveFrequencyCalibration-quot/m-p/230243#M4892</guid>
      <dc:creator>rabbit</dc:creator>
      <dc:date>2014-02-13T07:00:59Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 Serial Bootloader "SlaveFrequencyCalibration()"</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/AN2295-Serial-Bootloader-quot-SlaveFrequencyCalibration-quot/m-p/230244#M4893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rabbit,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SlaveFrequencyCalibration() is used to measures break impulse from PC and sets correct trim value, it firstly set UART RX pin as GPIO function and wait for the falling edge on it and then start to count the systick with the help of systick timer till it observes a rising edge on that pin, then it uses the result to calculate the trim value, but as the device doesn't support float point, so the final value might have some offset in some cases.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please kindly let me know if you have any further question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!!&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2014 06:52:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/AN2295-Serial-Bootloader-quot-SlaveFrequencyCalibration-quot/m-p/230244#M4893</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-02-18T06:52:48Z</dc:date>
    </item>
  </channel>
</rss>