<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Flash swap example for IAR/MQX</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-swap-example-for-IAR-MQX/m-p/230201#M4889</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mac,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply. Actually, there is no bootloader project in the mqx/examples/ folder (MQX 4.0).&lt;/P&gt;&lt;P&gt;Could you share it for us?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Apr 2013 16:00:16 GMT</pubDate>
    <dc:creator>artur73</dc:creator>
    <dc:date>2013-04-03T16:00:16Z</dc:date>
    <item>
      <title>Flash swap example for IAR/MQX</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-swap-example-for-IAR-MQX/m-p/230199#M4887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm looking for some code example to upload firmware to the K60 (through web preferably) and update the active flash image with this new image using swap feature. I use IAR with MQX.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I looked through the example AN4533, but this is not enough for me. I'm a bit new to Freescale programming, so any help will appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Mar 2013 19:50:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-swap-example-for-IAR-MQX/m-p/230199#M4887</guid>
      <dc:creator>artur73</dc:creator>
      <dc:date>2013-03-18T19:50:40Z</dc:date>
    </item>
    <item>
      <title>Re: Flash swap example for IAR/MQX</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-swap-example-for-IAR-MQX/m-p/230200#M4888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Some suggestions...&amp;nbsp; &lt;/P&gt;&lt;P&gt;There is a great thread here on how firmware update bootloader using flash swap can be added to MQX 4.0.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/315330"&gt;Using flashx io_ioctl FLASH_IOCTL_SWAP_FLASH_AND_RESET for bootloader&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an ethernet bootloader example available within MQX at /mqx/examples/bootloader/.&amp;nbsp; It uses TFTP to transfer a new firmware image over a network to program in memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should be able to piece together elements to implement an ethernet bootloader that uses the swapable flash blocks.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hope that helps.&lt;/P&gt;&lt;P&gt;Mac &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2013 19:44:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-swap-example-for-IAR-MQX/m-p/230200#M4888</guid>
      <dc:creator>macl</dc:creator>
      <dc:date>2013-03-21T19:44:01Z</dc:date>
    </item>
    <item>
      <title>Re: Flash swap example for IAR/MQX</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-swap-example-for-IAR-MQX/m-p/230201#M4889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mac,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply. Actually, there is no bootloader project in the mqx/examples/ folder (MQX 4.0).&lt;/P&gt;&lt;P&gt;Could you share it for us?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Apr 2013 16:00:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-swap-example-for-IAR-MQX/m-p/230201#M4889</guid>
      <dc:creator>artur73</dc:creator>
      <dc:date>2013-04-03T16:00:16Z</dc:date>
    </item>
  </channel>
</rss>