<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Why my crystal circuit for MKW01 not work in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-my-crystal-circuit-for-MKW01-not-work/m-p/802741#M48834</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi dear,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I design a MKW01Z128CHN board refer to KW01-9032 demo board and MKW01 datasheet Chapter 9 " &lt;SPAN class=""&gt;Typical Applications Circuit&lt;/SPAN&gt;", with a &lt;SPAN&gt;oscillation&amp;nbsp;circuit including a&amp;nbsp;&lt;/SPAN&gt;32MHz crystal (100ppm, 3225), two&amp;nbsp;11pF capacitance (C7 and C4, 0402).&amp;nbsp; I use 265&amp;nbsp;degrees heat gun to solder the MCU and&amp;nbsp;crystal manually.&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;Then&lt;/SPAN&gt;&lt;/SPAN&gt;&amp;nbsp;I found the clock circuit do not work as followed:&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. When I use J-Link, most time it cannot connect to target. Only&amp;nbsp;a few times I can flash the code into the target. When I use debug function, after download the code, it cannot start working.&lt;/P&gt;&lt;P&gt;2. When the MCU work standalone without J-Link, most time the &lt;SPAN&gt;crystal&lt;/SPAN&gt; cannot start oscillation. Some time I touch the board can start the&amp;nbsp;&lt;SPAN&gt;oscillation and the MCU will work OK.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Besides, I found VR_DIG and VR_ANA have no stable output.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can you help me to&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;analyze the&amp;nbsp;phenomenon: Is it (1) because of my solder artwork? Or (2) because of the parameter of C21 and C22? Or (3) because of my PCB layout&amp;nbsp;trace of&amp;nbsp;oscillation circuit?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The schematic diagram and PCB layout&amp;nbsp;are as attached, together with KDS Jlink config.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks a lot! Looking forward to your reply.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Nov 2018 03:47:09 GMT</pubDate>
    <dc:creator>luws</dc:creator>
    <dc:date>2018-11-27T03:47:09Z</dc:date>
    <item>
      <title>Why my crystal circuit for MKW01 not work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-my-crystal-circuit-for-MKW01-not-work/m-p/802741#M48834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi dear,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I design a MKW01Z128CHN board refer to KW01-9032 demo board and MKW01 datasheet Chapter 9 " &lt;SPAN class=""&gt;Typical Applications Circuit&lt;/SPAN&gt;", with a &lt;SPAN&gt;oscillation&amp;nbsp;circuit including a&amp;nbsp;&lt;/SPAN&gt;32MHz crystal (100ppm, 3225), two&amp;nbsp;11pF capacitance (C7 and C4, 0402).&amp;nbsp; I use 265&amp;nbsp;degrees heat gun to solder the MCU and&amp;nbsp;crystal manually.&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;Then&lt;/SPAN&gt;&lt;/SPAN&gt;&amp;nbsp;I found the clock circuit do not work as followed:&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. When I use J-Link, most time it cannot connect to target. Only&amp;nbsp;a few times I can flash the code into the target. When I use debug function, after download the code, it cannot start working.&lt;/P&gt;&lt;P&gt;2. When the MCU work standalone without J-Link, most time the &lt;SPAN&gt;crystal&lt;/SPAN&gt; cannot start oscillation. Some time I touch the board can start the&amp;nbsp;&lt;SPAN&gt;oscillation and the MCU will work OK.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Besides, I found VR_DIG and VR_ANA have no stable output.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can you help me to&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;analyze the&amp;nbsp;phenomenon: Is it (1) because of my solder artwork? Or (2) because of the parameter of C21 and C22? Or (3) because of my PCB layout&amp;nbsp;trace of&amp;nbsp;oscillation circuit?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The schematic diagram and PCB layout&amp;nbsp;are as attached, together with KDS Jlink config.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks a lot! Looking forward to your reply.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Nov 2018 03:47:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-my-crystal-circuit-for-MKW01-not-work/m-p/802741#M48834</guid>
      <dc:creator>luws</dc:creator>
      <dc:date>2018-11-27T03:47:09Z</dc:date>
    </item>
    <item>
      <title>Re: Why my crystal circuit for MKW01 not work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-my-crystal-circuit-for-MKW01-not-work/m-p/802742#M48835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Hi Wenshaui,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;EM style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: inherit;"&gt;Besides, I found VR_DIG and VR_ANA have no stable output.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;This output value is not recommended for reference on your circuit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Dec 2018 21:29:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-my-crystal-circuit-for-MKW01-not-work/m-p/802742#M48835</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2018-12-04T21:29:06Z</dc:date>
    </item>
  </channel>
</rss>