<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKinetisFlashTool for KE18F</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KinetisFlashTool-for-KE18F/m-p/801322#M48732</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Kinetis bootloader is the program residing in the on-chip read-only memory (ROM)&lt;BR /&gt;of a Kinetis microcontroller device. There is hardware logic in place at boot time that&lt;BR /&gt;either starts execution of an embedded image available on the internal flash memory, or&lt;BR /&gt;starts the execution of the Kinetis Bootloader from on-chip ROM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;• FOPT [7] is set to 1. This forces the ROM to run out of reset.&lt;BR /&gt;• The BOOTCFG0 pin is asserted. The pin must be configured as BOOTCFG0 by&lt;BR /&gt;setting the BOOTPIN_OPT bit of FOPT to 0.&lt;BR /&gt;• A user applications running on flash or RAM calls into the Kinetis Bootloader entry&lt;BR /&gt;point address in ROM, to start Kinetis Bootloader execution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63088i133AD22E7C5909B6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63134iE6E0650A083E4C48/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;How to config the MKE18F512VLL16 to use the KinetisFlashTool?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 19 Aug 2018 04:35:54 GMT</pubDate>
    <dc:creator>lifeng</dc:creator>
    <dc:date>2018-08-19T04:35:54Z</dc:date>
    <item>
      <title>KinetisFlashTool for KE18F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KinetisFlashTool-for-KE18F/m-p/801322#M48732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Kinetis bootloader is the program residing in the on-chip read-only memory (ROM)&lt;BR /&gt;of a Kinetis microcontroller device. There is hardware logic in place at boot time that&lt;BR /&gt;either starts execution of an embedded image available on the internal flash memory, or&lt;BR /&gt;starts the execution of the Kinetis Bootloader from on-chip ROM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;• FOPT [7] is set to 1. This forces the ROM to run out of reset.&lt;BR /&gt;• The BOOTCFG0 pin is asserted. The pin must be configured as BOOTCFG0 by&lt;BR /&gt;setting the BOOTPIN_OPT bit of FOPT to 0.&lt;BR /&gt;• A user applications running on flash or RAM calls into the Kinetis Bootloader entry&lt;BR /&gt;point address in ROM, to start Kinetis Bootloader execution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63088i133AD22E7C5909B6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63134iE6E0650A083E4C48/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;How to config the MKE18F512VLL16 to use the KinetisFlashTool?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Aug 2018 04:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KinetisFlashTool-for-KE18F/m-p/801322#M48732</guid>
      <dc:creator>lifeng</dc:creator>
      <dc:date>2018-08-19T04:35:54Z</dc:date>
    </item>
    <item>
      <title>Re: KinetisFlashTool for KE18F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KinetisFlashTool-for-KE18F/m-p/801323#M48733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63175iD24154DEA56C4B18/image-size/large?v=v2&amp;amp;px=999" title="temp.png" alt="temp.png" /&gt;&lt;/span&gt;Hi Li,&lt;/P&gt;&lt;P&gt;If you use TWR-KE18F, just connect&amp;nbsp; the usb port to computer. Then select&amp;nbsp; the UART port which create by the openSDA serial and debug adaptor,&amp;nbsp;press the reset button, and click the Connect button. The tool will try to connect to the board. Baudrate is not important.&lt;/P&gt;&lt;P&gt;If you use your own board, you should connect your computer to the LPUART port which list on page 565 in reference manual.&lt;/P&gt;&lt;P&gt;If the connection can't established, you can make a full erase. Then it will be ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Aug 2018 04:15:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KinetisFlashTool-for-KE18F/m-p/801323#M48733</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2018-08-20T04:15:53Z</dc:date>
    </item>
    <item>
      <title>Re: KinetisFlashTool for KE18F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KinetisFlashTool-for-KE18F/m-p/801324#M48734</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;For&amp;nbsp;&amp;nbsp;TWR-KE18F,&amp;nbsp; connect&amp;nbsp; the usb port to computer. Then select&amp;nbsp; the UART port which create by the openSDA serial and debug adaptor,&amp;nbsp;press the reset button &lt;STRONG&gt;and sw2 button&lt;/STRONG&gt;(PTD3,NMI, BOOTCFG0), &lt;STRONG&gt;release reset button and hold sw2 pressing and click the Connect button&lt;/STRONG&gt;. The tool will try to connect to the board. Baudrate is not important.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Oct 2018 10:46:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KinetisFlashTool-for-KE18F/m-p/801324#M48734</guid>
      <dc:creator>lifeng</dc:creator>
      <dc:date>2018-10-03T10:46:44Z</dc:date>
    </item>
  </channel>
</rss>