<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: FRDM-K64 PIN Digital Read</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-PIN-Digital-Read/m-p/799373#M48598</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Antonio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If a pin is configured as GPIO (with clock gated to it) and its GPIOx_PDDR is '0' you can read its state in the GPIOx_PDIR register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't have the impression that developers using the NXP forum use Arduino so you may find more suitable answers to your environment at the Teensy forum - the TEENSY 3.5 uses the K64.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case you are making a transition from the Arduino world you can try the uTasker project (open source on Git Hub) since it also supports TEENSy 3.5 (and FRDM-K64F etc.), including simulation of the device/board so that you can more easily learn the internal workings. It doesn't constrain you to a certain environment since it is neutral and includes project for most common IDEs (MCUXpresso, CW, KDS, IAR, Keil, Rowley, Atollic, etc...).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Oct 2018 00:02:54 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2018-10-17T00:02:54Z</dc:date>
    <item>
      <title>FRDM-K64 PIN Digital Read</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-PIN-Digital-Read/m-p/799372#M48597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I have a simple question. How do I use the DigtialRead function from Arduino in my FRMD K64 in C?. I need to read either high or low (1 | 0). I was&amp;nbsp;trying this with the GPIOx_PDIR function but this doesn't write you a Logic 0 when the read is 0.&lt;/P&gt;&lt;P&gt;Can anyone help me out?&lt;/P&gt;&lt;P&gt;Thank you very much.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Oct 2018 23:23:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-PIN-Digital-Read/m-p/799372#M48597</guid>
      <dc:creator>antonioangelm24</dc:creator>
      <dc:date>2018-10-16T23:23:24Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64 PIN Digital Read</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-PIN-Digital-Read/m-p/799373#M48598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Antonio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If a pin is configured as GPIO (with clock gated to it) and its GPIOx_PDDR is '0' you can read its state in the GPIOx_PDIR register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't have the impression that developers using the NXP forum use Arduino so you may find more suitable answers to your environment at the Teensy forum - the TEENSY 3.5 uses the K64.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case you are making a transition from the Arduino world you can try the uTasker project (open source on Git Hub) since it also supports TEENSy 3.5 (and FRDM-K64F etc.), including simulation of the device/board so that you can more easily learn the internal workings. It doesn't constrain you to a certain environment since it is neutral and includes project for most common IDEs (MCUXpresso, CW, KDS, IAR, Keil, Rowley, Atollic, etc...).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2018 00:02:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-PIN-Digital-Read/m-p/799373#M48598</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-10-17T00:02:54Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64 PIN Digital Read</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-PIN-Digital-Read/m-p/799374#M48599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answer. I'll get to that, and will check the uTasker you mencioned.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Oct 2018 00:06:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-PIN-Digital-Read/m-p/799374#M48599</guid>
      <dc:creator>antonioangelm24</dc:creator>
      <dc:date>2018-10-18T00:06:45Z</dc:date>
    </item>
  </channel>
</rss>