<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can i use 8 bit data out external SDRAM for updating graphics framebuffer (480x272, 16 bits color data) in kinetis K80 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798401#M48577</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hui_Ma..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot.. Got your attachment! Will go through the same..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Aug 2018 06:19:09 GMT</pubDate>
    <dc:creator>divyaece2</dc:creator>
    <dc:date>2018-08-24T06:19:09Z</dc:date>
    <item>
      <title>Can i use 8 bit data out external SDRAM for updating graphics framebuffer (480x272, 16 bits color data) in kinetis K80</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798395#M48571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using color TFT display with resolution 480x272 and color data is 565 RGB ie. 16 bits per pixel. i want to use FLEXIO to drive the LCD and&amp;nbsp; 8 bit data out SDRAM for graphics frame buffer because i have issue with pin count for 16 bit SDRAM.&lt;/P&gt;&lt;P&gt;Can i use 8 bit SDRAM insted of 16 bit for graphics frame buffer ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2018 07:31:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798395#M48571</guid>
      <dc:creator>pravin_patil</dc:creator>
      <dc:date>2018-08-17T07:31:05Z</dc:date>
    </item>
    <item>
      <title>Re: Can i use 8 bit data out external SDRAM for updating graphics framebuffer (480x272, 16 bits color data) in kinetis K80</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798396#M48572</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The &lt;A href="https://www.nxp.com/docs/en/application-note/AN5280.pdf"&gt;AN5280&lt;/A&gt;(Using Kinetis FlexIO to drive a graphical LCD) chapter 5 shows FlexIO_LCD bus bandwidth performance.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63231iD5A16D63EE1BDD4C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If there couldn't using 16-bit data port to access SDRAM, the FlexIO_LCD maximum bus bandwidth from SDRAM should below 31MBytes/s.&lt;/P&gt;&lt;P&gt;I don't know the LCD display pixel clock frequency (MHz), you could check with LCD display datasheet to get that data.&lt;/P&gt;&lt;P&gt;Please calculate if the FlexIO_LCD bus bandwidth could match with that LCD display requirement.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Aug 2018 09:02:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798396#M48572</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2018-08-20T09:02:24Z</dc:date>
    </item>
    <item>
      <title>Re: Can i use 8 bit data out external SDRAM for updating graphics framebuffer (480x272, 16 bits color data) in kinetis K80</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798397#M48573</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi..&lt;/P&gt;&lt;P&gt;I have the same issue as Parvin Patil mentioned but the difference is that internal SDRAM. Now I am working on IMX RT-1050 for updating graphics frame buffer (480 x 272). I am a beginner with that.. Please, give me the example for accessing the sdram of imxrt 1050. It would be helpful for me...&lt;/P&gt;&lt;H1&gt;&lt;/H1&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Divya.S&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Aug 2018 13:38:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798397#M48573</guid>
      <dc:creator>divyaece2</dc:creator>
      <dc:date>2018-08-20T13:38:30Z</dc:date>
    </item>
    <item>
      <title>Re: Can i use 8 bit data out external SDRAM for updating graphics framebuffer (480x272, 16 bits color data) in kinetis K80</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798398#M48574</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the MCUXpresso SDK software package for i.MX RT1050 with SDRAM initialization code at &amp;lt;evkbimxrt1050_sdram_init.mac&amp;gt; file, which will be called during SDRAM target project debugger process.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67132i84A8B6BBFAB22558/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I attached that file for your reference.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Aug 2018 02:23:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798398#M48574</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2018-08-21T02:23:02Z</dc:date>
    </item>
    <item>
      <title>Re: Can i use 8 bit data out external SDRAM for updating graphics framebuffer (480x272, 16 bits color data) in kinetis K80</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798399#M48575</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Hui_Ma...&lt;/P&gt;&lt;P&gt;Thank you so much for support.. But I can't find your attachment file. And where can I find the factory settings in mcuxpresso IDE.. Please send your response as soon as possible...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Aug 2018 07:02:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798399#M48575</guid>
      <dc:creator>divyaece2</dc:creator>
      <dc:date>2018-08-23T07:02:34Z</dc:date>
    </item>
    <item>
      <title>Re: Can i use 8 bit data out external SDRAM for updating graphics framebuffer (480x272, 16 bits color data) in kinetis K80</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798400#M48576</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you need to change another browser software (such as IE or Firefox) to check the attachment.&lt;/P&gt;&lt;P&gt;Please check &lt;A _jive_internal="true" href="https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide/blog/2017/12/07/overview-of-using-the-mimxrt1050-evk-with-mcuxpresso-ide"&gt;here&lt;/A&gt; about Overview i.MXRT1050 with MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Aug 2018 08:15:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798400#M48576</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2018-08-23T08:15:37Z</dc:date>
    </item>
    <item>
      <title>Re: Can i use 8 bit data out external SDRAM for updating graphics framebuffer (480x272, 16 bits color data) in kinetis K80</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798401#M48577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hui_Ma..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot.. Got your attachment! Will go through the same..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Aug 2018 06:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-i-use-8-bit-data-out-external-SDRAM-for-updating-graphics/m-p/798401#M48577</guid>
      <dc:creator>divyaece2</dc:creator>
      <dc:date>2018-08-24T06:19:09Z</dc:date>
    </item>
  </channel>
</rss>