<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Kinetis MK66, DMA to read GPIO</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797788#M48530</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, I will use PDIR.&lt;/P&gt;&lt;P&gt;Sorry, but I do not understand how trigger the DMA with six signals (GPIO pins), if possible, to capture my data bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand that the limit of DMA trigger is one signal, then I can not use six different signals (GPIO input pins) to trigger same DMA to capture 8 GPIO pins. Or I have misunderstood what is the DMA trigger limit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 24 Nov 2018 03:55:54 GMT</pubDate>
    <dc:creator>luishs</dc:creator>
    <dc:date>2018-11-24T03:55:54Z</dc:date>
    <item>
      <title>Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797783#M48525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I try to use DMA to read several GPIO pins, but in the SDK there is no example of source code. I found the AN4627SW source code in Google (attached), but if I copy it to my current MK66 project, there are many errors when compiling. Most errors are "undeclared", it seems that it is not for Kinetis MK66 and I do not know how to port it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the MK66 SDK there are two examples of source code, memory to memory, I'm not sure if&amp;nbsp;I could use them simply by modifying the source address so that it points to the GPIO port address instead of to an address of the RAM (data array) ).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Can someone help me, with some source code for Kinetis MK66, using DMA to read 8 pins of the GPIO port, activated by several external signals? Basically I have an 8-bit data bus, which I need to capture and process, activated by various data from a control bus.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Nov 2018 18:10:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797783#M48525</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2018-11-23T18:10:39Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797784#M48526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Luis&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the uTasker project it is done like this (assuming triggered by the falling edge of PTB16):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="property macro token"&gt;#define OUTPUT_LENGTH&amp;nbsp; 100&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;long&lt;/SPAN&gt; ulOutput&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;OUTPUT_LENGTH&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;fnSampleBus&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp; INTERRUPT_SETUP interrupt_setup&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// interrupt configuration parameters&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;int_type &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; PORT_INTERRUPT&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// identifier to configure port interrupt&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;int_port &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; PORTB&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// the port that the interrupt input is on&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;int_port_bits &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; PORTB_BIT16&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// UART input pin on FRDM-K64F&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;int_port_sense &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;IRQ_FALLING_EDGE &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; PULLUP_ON &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; PORT_DMA_MODE&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// DMA on falling edge&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;int_handler &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// no interrupt handler when using DMA&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;fnConfigureInterrupt&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;interrupt_setup&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// configure interrupt&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// Configure the DMA trigger&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;//&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;fnConfigDMA_buffer&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;9&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; DMAMUX0_CHCFG_SOURCE_PORTB&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;sizeof&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;ulOutput&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;GPIO_REGS &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;GPIOC_ADD&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;PDIR&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;ulOutput&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;DMA_DIRECTION_INPUT &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; DMA_LONG_WORDS&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// use DMA channel 9 without any interrupts&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;fnDMA_BufferReset&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;9&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; DMA_BUFFER_START&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;It will fill the buffer ulOutput[] with the PORTC input value on each edge.&lt;BR /&gt;Bytes (instead of the complete port width) can be copied using DMA_BYTES flag instead (byte buffer)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code is on GitHub and is compatible with all Kinetis parts with port DMA capability (including K66).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Beware that only one DMA trigger is possible per port. Therefore, for example, maximum 5 different DMA port triggers would be possible on a part with DMA capability on ports A, B, C, D and E.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Nov 2018 21:42:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797784#M48526</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-11-23T21:42:23Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797785#M48527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks mark.&lt;/P&gt;&lt;P&gt;Then it is not possible to trigger the GPIO data capture, using several ports as triggers to capture the same GPIO data (8 pins)?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;The problem is that I have an 8 bit data bus, and a 6 signal control bus. Each time one of these 6 signals is set to a low logic level, it tells me that I have data on the data bus, and that I must capture it.&lt;/P&gt;&lt;P&gt;I thought I could do it with the DMA, but for that I must be able to trigger the capture of the 8 pins of the data bus, with 6 different signals from my control bus.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Is it not possible to do this with the DMA, is only a hardware signal possible to trigger the DMA?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Nov 2018 23:11:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797785#M48527</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2018-11-23T23:11:59Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797786#M48528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm thinking that maybe I could do it using only interrupts, instead of the DMA.&amp;nbsp;I tried with interrupts, but I'm not sure if I could read several GPIO pins with a single instruction.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;These are the pins that I have assigned to my data bus.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;D0 -&amp;gt; PTA15&lt;BR /&gt;&amp;nbsp;&amp;nbsp;D1 -&amp;gt; PTA14&lt;BR /&gt;&amp;nbsp;&amp;nbsp;D2 -&amp;gt; PTA13&lt;BR /&gt;&amp;nbsp;&amp;nbsp;D3 -&amp;gt; PTA12&lt;BR /&gt;&amp;nbsp;&amp;nbsp;D4 -&amp;gt; PTA11&lt;BR /&gt;&amp;nbsp;&amp;nbsp;D5 -&amp;gt; PTA10&lt;BR /&gt;&amp;nbsp;&amp;nbsp;D6 -&amp;gt; PTA9&lt;BR /&gt;&amp;nbsp;&amp;nbsp;D7 -&amp;gt; PTA8&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;And to read each pin I use eight instructions, one to read each pin:&lt;/P&gt;&lt;P&gt;#define LEE_D0 GPIO_PinRead (BOARD_INITPINS_D0_GPIO, BOARD_INITPINS_D0_PIN)&lt;BR /&gt;#define LEE_D1 GPIO_PinRead (BOARD_INITPINS_D1_GPIO, BOARD_INITPINS_D1_PIN)&lt;BR /&gt;#define LEE_D2 GPIO_PinRead (BOARD_INITPINS_D2_GPIO, BOARD_INITPINS_D2_PIN)&lt;BR /&gt;#define LEE_D3 GPIO_PinRead (BOARD_INITPINS_D3_GPIO, BOARD_INITPINS_D3_PIN)&lt;BR /&gt;#define LEE_D4 GPIO_PinRead (BOARD_INITPINS_D4_GPIO, BOARD_INITPINS_D4_PIN)&lt;BR /&gt;#define LEE_D5 GPIO_PinRead (BOARD_INITPINS_D5_GPIO, BOARD_INITPINS_D5_PIN)&lt;BR /&gt;#define LEE_D6 GPIO_PinRead (BOARD_INITPINS_D6_GPIO, BOARD_INITPINS_D6_PIN)&lt;BR /&gt;#define LEE_D7 GPIO_PinRead (BOARD_INITPINS_D7_GPIO, BOARD_INITPINS_D7_PIN)&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Do you know if I could read the 8 pins of the same port, with a single instruction, instead of having to do 8 readings, one for each pin?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;The idea is that 6 signals from my control bus, trigger interrupts, and in the interrupt routine, detecting which pin triggered the interrupt, I read the GPIO with the data of my data bus and I keep it for its process (show status of each data in several Led matrix). Now I do 8 readings, to read each one the 8 bits of the data bus assigned each to a pin of the microcontroller.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;The signals do not think they are very fast, since it is an arcade machine from the 90s, with an EF68B09EP processor at 8Mhz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Nov 2018 00:23:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797786#M48528</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2018-11-24T00:23:05Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797787#M48529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Luis&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The DMA triggers are limited and not the reading.&lt;/P&gt;&lt;PRE class=""&gt;&lt;CODE&gt;unsigned char ucDataBus = (unsigned char)(GPIOA_&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;PDIR &amp;gt; 8);&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;is all that you need to read your 8 bit bus input.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The DMA case simply puts it into a variable for you on each trigger without needing an interrupt each time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Nov 2018 01:31:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797787#M48529</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-11-24T01:31:02Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797788#M48530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, I will use PDIR.&lt;/P&gt;&lt;P&gt;Sorry, but I do not understand how trigger the DMA with six signals (GPIO pins), if possible, to capture my data bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand that the limit of DMA trigger is one signal, then I can not use six different signals (GPIO input pins) to trigger same DMA to capture 8 GPIO pins. Or I have misunderstood what is the DMA trigger limit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Nov 2018 03:55:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797788#M48530</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2018-11-24T03:55:54Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797789#M48531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;About your suggestion using&amp;nbsp;&amp;nbsp;&lt;CODE style="border: 0px; font-weight: inherit;"&gt;unsigned char ucDataBus = (unsigned char)(GPIOA_&lt;SPAN class="" style="border: 0px; font-weight: inherit;"&gt;&lt;/SPAN&gt;&lt;SPAN class="" style="border: 0px; font-weight: inherit;"&gt;&lt;/SPAN&gt;PDIR &amp;gt; 8);&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is it possible to read the status of each pin, with only one GPIO reading, to load them into an array of 8 elements?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE style="border: 0px; font-weight: inherit;"&gt;&lt;/CODE&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Nov 2018 05:43:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797789#M48531</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2018-11-24T05:43:03Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797790#M48532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have put your instruction&amp;nbsp;&lt;CODE style="border: 0px; font-weight: inherit; font-size: 14px;"&gt;unsigned char ucDataBus = (unsigned char)(GPIOA_&lt;SPAN class="" style="border: 0px; font-weight: inherit; font-size: 14px;"&gt;&lt;/SPAN&gt;&lt;SPAN class="" style="border: 0px; font-weight: inherit; font-size: 14px;"&gt;&lt;/SPAN&gt;PDIR &amp;gt; 8);&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;in my program, but compiler fail, show this error message&amp;nbsp;" error: 'GPIOA_PDIR' undeclared (first use in this function); did you mean 'GPIOA_BASE'? "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have replace it by this, and compile with success:&lt;/P&gt;&lt;P&gt;unsigned char ucDataBus = (unsigned char)(GPIOA-&amp;gt;PDIR &amp;gt; 8);&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Nov 2018 06:12:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797790#M48532</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2018-11-24T06:12:21Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797791#M48533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Luis&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact there is just one DMA trigger source for a port but you could set all of your 6 inputs &lt;SPAN style="text-decoration: underline;"&gt;to the same trigger&lt;/SPAN&gt; if any of them falling low needs to generate the same event.&lt;/P&gt;&lt;P&gt;In the uTasker code it is done by (assuming the 6 inputs on the same port on PTB16..PTB21)&lt;/P&gt;&lt;PRE class=""&gt;&lt;CODE&gt;
&lt;/CODE&gt;&lt;CODE&gt;
&lt;/CODE&gt;&lt;CODE&gt;PORTB_BIT18 | &lt;/CODE&gt;&lt;CODE&gt;
&lt;/CODE&gt;&lt;CODE&gt; | &lt;/CODE&gt;&lt;CODE&gt;PORTB_BIT20&lt;/CODE&gt;&lt;CODE&gt;)&lt;SPAN class=""&gt;;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;The method used to address peripheral registers depends on the library used. In the uTasker project&amp;nbsp;&lt;CODE style="border: 0px; font-weight: inherit; font-size: 14px;"&gt;GPIOA_&lt;SPAN class="" style="border: 0px; font-weight: inherit; font-size: 14px;"&gt;&lt;/SPAN&gt;&lt;SPAN class="" style="border: 0px; font-weight: inherit; font-size: 14px;"&gt;&lt;/SPAN&gt;PDIR&lt;/CODE&gt;&amp;nbsp; is used .&lt;CODE style="border: 0px; font-weight: inherit; font-size: 14px;"&gt;&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The major advantage of the uTasker method is that it also allows compete simulation of the operation so the above code can be verified without the need for HW (and in a much more efficient debugging environment).&lt;/P&gt;&lt;P&gt;I have attached a short video showing the code in operation. It shows setting some port input states on port C, triggering DMA by falling edges on the 6 port B inputs and checking that the DMA transfers have been made by looking at the capture buffer in a watch window.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you see it is possible to do with around 10 lines of intuitive user code and verify operation within a minute or so, making it much more efficient than the traditional library and development methods. It allows professional developers to greatly reduce costs; whereas typical developers spend hours or days working out how it operates internally and experimenting with changes to example code to get it working uTasker developers can quickly complete their development so that they are already selling their product while others are still fighting with the details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Nov 2018 13:11:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797791#M48533</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-11-24T13:11:48Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797792#M48534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much for the clarification Mark, now I understand.&lt;/P&gt;&lt;P&gt;So this is going to be very useful for what I need to program.&lt;/P&gt;&lt;P&gt;Thanks for your help, I'm going to try it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Nov 2018 13:21:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797792#M48534</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2018-11-24T13:21:23Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797793#M48535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Some questions, about your code, please.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.- When some of the six GPIO signals trigger the DMA, how do I detect it in my program, to copy and use the data stored by the DMA in the output variable ?, is a Flag activated or the program must jump to any routine with a special name, such as when a pin interrupt is configured?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.- Is there a way to know which of the six signals was the one that triggered the DMA?, I will need it to be able to identify and process that data, according to which signal of the control bus&amp;nbsp;triggered&amp;nbsp;the capture of data from the data bus.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;3.- The configuration that you put of the DMA, need some additional instruction to start or stop the DMA?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Nov 2018 13:46:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797793#M48535</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2018-11-24T13:46:20Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797794#M48536</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have compile your source code but there are a lot of errors. I do not know what is the problem, probably you work with a different library, or I need add some library to my project.&amp;nbsp;I work with MCUXpresso and SDK source examples to start this project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are the errors when I try to compile your source code:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;../source/pit.c:423:5: error: unknown type name 'INTERRUPT_SETUP'&lt;BR /&gt; INTERRUPT_SETUP interrupt_setup; // interrupt configuration parameters&lt;BR /&gt; ^~~~~~~~~~~~~~~&lt;BR /&gt;../source/pit.c:424:20: error: request for member 'int_type' in something not a structure or union&lt;BR /&gt; interrupt_setup.int_type = PORT_INTERRUPT; // identifier to configure port interrupt&lt;BR /&gt; ^&lt;BR /&gt;../source/pit.c:424:32: error: 'PORT_INTERRUPT' undeclared (first use in this function); did you mean 'PORT_DFER_DFE'?&lt;BR /&gt; interrupt_setup.int_type = PORT_INTERRUPT; // identifier to configure port interrupt&lt;BR /&gt; ^~~~~~~~~~~~~~&lt;BR /&gt; PORT_DFER_DFE&lt;BR /&gt;../source/pit.c:424:32: note: each undeclared identifier is reported only once for each function it appears in&lt;BR /&gt;../source/pit.c:425:20: error: request for member 'int_port' in something not a structure or union&lt;BR /&gt; interrupt_setup.int_port = PORTB; // the port that the interrupt input is on&lt;BR /&gt; ^&lt;BR /&gt;../source/pit.c:427:20: error: request for member 'int_port_bits' in something not a structure or union&lt;BR /&gt; interrupt_setup.int_port_bits = PORTB_BIT16; // UART input pin on FRDM-K64F&lt;BR /&gt; ^&lt;BR /&gt;../source/pit.c:427:37: error: 'PORTB_BIT16' undeclared (first use in this function); did you mean 'PORTB_IRQn'?&lt;BR /&gt; interrupt_setup.int_port_bits = PORTB_BIT16; // UART input pin on FRDM-K64F&lt;BR /&gt; ^~~~~~~~~~~&lt;BR /&gt; PORTB_IRQn&lt;BR /&gt;../source/pit.c:429:20: error: request for member 'int_port_bits' in something not a structure or union&lt;BR /&gt; interrupt_setup.int_port_bits = (PORTB_BIT16 | PORTB_BIT17 | PORTB_BIT18 | PORTB_BIT19 | PORTB_BIT20);&lt;BR /&gt; ^&lt;BR /&gt;../source/pit.c:429:52: error: 'PORTB_BIT17' undeclared (first use in this function); did you mean 'PORTB_BIT16'?&lt;BR /&gt; interrupt_setup.int_port_bits = (PORTB_BIT16 | PORTB_BIT17 | PORTB_BIT18 | PORTB_BIT19 | PORTB_BIT20);&lt;BR /&gt; ^~~~~~~~~~~&lt;BR /&gt; PORTB_BIT16&lt;BR /&gt;../source/pit.c:429:66: error: 'PORTB_BIT18' undeclared (first use in this function); did you mean 'PORTB_BIT17'?&lt;BR /&gt; interrupt_setup.int_port_bits = (PORTB_BIT16 | PORTB_BIT17 | PORTB_BIT18 | PORTB_BIT19 | PORTB_BIT20);&lt;BR /&gt; ^~~~~~~~~~~&lt;BR /&gt; PORTB_BIT17&lt;BR /&gt;../source/pit.c:429:80: error: 'PORTB_BIT19' undeclared (first use in this function); did you mean 'PORTB_BIT18'?&lt;BR /&gt; interrupt_setup.int_port_bits = (PORTB_BIT16 | PORTB_BIT17 | PORTB_BIT18 | PORTB_BIT19 | PORTB_BIT20);&lt;BR /&gt; ^~~~~~~~~~~&lt;BR /&gt; PORTB_BIT18&lt;BR /&gt;../source/pit.c:429:94: error: 'PORTB_BIT20' undeclared (first use in this function); did you mean 'PORTB_BIT19'?&lt;BR /&gt; interrupt_setup.int_port_bits = (PORTB_BIT16 | PORTB_BIT17 | PORTB_BIT18 | PORTB_BIT19 | PORTB_BIT20);&lt;BR /&gt; ^~~~~~~~~~~&lt;BR /&gt; PORTB_BIT19&lt;BR /&gt;../source/pit.c:431:20: error: request for member 'int_port_sense' in something not a structure or union&lt;BR /&gt; interrupt_setup.int_port_sense = (IRQ_FALLING_EDGE | PULLUP_ON | PORT_DMA_MODE); // DMA on falling edge&lt;BR /&gt; ^&lt;BR /&gt;../source/pit.c:431:39: error: 'IRQ_FALLING_EDGE' undeclared (first use in this function)&lt;BR /&gt; interrupt_setup.int_port_sense = (IRQ_FALLING_EDGE | PULLUP_ON | PORT_DMA_MODE); // DMA on falling edge&lt;BR /&gt; ^~~~~~~~~~~~~~~~&lt;BR /&gt;../source/pit.c:431:58: error: 'PULLUP_ON' undeclared (first use in this function)&lt;BR /&gt; interrupt_setup.int_port_sense = (IRQ_FALLING_EDGE | PULLUP_ON | PORT_DMA_MODE); // DMA on falling edge&lt;BR /&gt; ^~~~~~~~~&lt;BR /&gt;../source/pit.c:431:70: error: 'PORT_DMA_MODE' undeclared (first use in this function); did you mean 'PORT_PCR_ODE'?&lt;BR /&gt; interrupt_setup.int_port_sense = (IRQ_FALLING_EDGE | PULLUP_ON | PORT_DMA_MODE); // DMA on falling edge&lt;BR /&gt; ^~~~~~~~~~~~~&lt;BR /&gt; PORT_PCR_ODE&lt;BR /&gt;../source/pit.c:432:20: error: request for member 'int_handler' in something not a structure or union&lt;BR /&gt; interrupt_setup.int_handler = 0; // no interrupt handler when using DMA&lt;BR /&gt; ^&lt;BR /&gt;../source/pit.c:433:5: warning: implicit declaration of function 'fnConfigureInterrupt' [-Wimplicit-function-declaration]&lt;BR /&gt; fnConfigureInterrupt((void *)&amp;amp;interrupt_setup); // configure interrupt&lt;BR /&gt; ^~~~~~~~~~~~~~~~~~~~&lt;BR /&gt;../source/pit.c:436:5: warning: implicit declaration of function 'fnConfigDMA_buffer' [-Wimplicit-function-declaration]&lt;BR /&gt; fnConfigDMA_buffer(9, DMAMUX0_CHCFG_SOURCE_PORTB, sizeof(ulOutput), (void *)&amp;amp;(((GPIO_REGS *)GPIOC_ADD)-&amp;gt;PDIR), (void *)&amp;amp;ulOutput, (DMA_DIRECTION_INPUT | DMA_LONG_WORDS), 0, 0); // use DMA channel 9 without any interrupts&lt;BR /&gt; ^~~~~~~~~~~~~~~~~~&lt;BR /&gt;../source/pit.c:436:27: error: 'DMAMUX0_CHCFG_SOURCE_PORTB' undeclared (first use in this function); did you mean 'DMAMUX_CHCFG_SOURCE_SHIFT'?&lt;BR /&gt; fnConfigDMA_buffer(9, DMAMUX0_CHCFG_SOURCE_PORTB, sizeof(ulOutput), (void *)&amp;amp;(((GPIO_REGS *)GPIOC_ADD)-&amp;gt;PDIR), (void *)&amp;amp;ulOutput, (DMA_DIRECTION_INPUT | DMA_LONG_WORDS), 0, 0); // use DMA channel 9 without any interrupts&lt;BR /&gt; ^~~~~~~~~~~~~~~~~~~~~~~~~~&lt;BR /&gt; DMAMUX_CHCFG_SOURCE_SHIFT&lt;BR /&gt;../source/pit.c:436:85: error: 'GPIO_REGS' undeclared (first use in this function); did you mean 'GPIO_Type'?&lt;BR /&gt; fnConfigDMA_buffer(9, DMAMUX0_CHCFG_SOURCE_PORTB, sizeof(ulOutput), (void *)&amp;amp;(((GPIO_REGS *)GPIOC_ADD)-&amp;gt;PDIR), (void *)&amp;amp;ulOutput, (DMA_DIRECTION_INPUT | DMA_LONG_WORDS), 0, 0); // use DMA channel 9 without any interrupts&lt;BR /&gt; ^~~~~~~~~&lt;BR /&gt; GPIO_Type&lt;BR /&gt;../source/pit.c:436:96: error: expected expression before ')' token&lt;BR /&gt; fnConfigDMA_buffer(9, DMAMUX0_CHCFG_SOURCE_PORTB, sizeof(ulOutput), (void *)&amp;amp;(((GPIO_REGS *)GPIOC_ADD)-&amp;gt;PDIR), (void *)&amp;amp;ulOutput, (DMA_DIRECTION_INPUT | DMA_LONG_WORDS), 0, 0); // use DMA channel 9 without any interrupts&lt;BR /&gt; ^&lt;BR /&gt;../source/pit.c:436:136: error: 'DMA_DIRECTION_INPUT' undeclared (first use in this function)&lt;BR /&gt; fnConfigDMA_buffer(9, DMAMUX0_CHCFG_SOURCE_PORTB, sizeof(ulOutput), (void *)&amp;amp;(((GPIO_REGS *)GPIOC_ADD)-&amp;gt;PDIR), (void *)&amp;amp;ulOutput, (DMA_DIRECTION_INPUT | DMA_LONG_WORDS), 0, 0); // use DMA channel 9 without any interrupts&lt;BR /&gt; ^~~~~~~~~~~~~~~~~~~&lt;BR /&gt;../source/pit.c:436:158: error: 'DMA_LONG_WORDS' undeclared (first use in this function); did you mean 'DMA_CHN_IRQS'?&lt;BR /&gt; fnConfigDMA_buffer(9, DMAMUX0_CHCFG_SOURCE_PORTB, sizeof(ulOutput), (void *)&amp;amp;(((GPIO_REGS *)GPIOC_ADD)-&amp;gt;PDIR), (void *)&amp;amp;ulOutput, (DMA_DIRECTION_INPUT | DMA_LONG_WORDS), 0, 0); // use DMA channel 9 without any interrupts&lt;BR /&gt; ^~~~~~~~~~~~~~&lt;BR /&gt; DMA_CHN_IRQS&lt;BR /&gt;../source/pit.c:437:5: warning: implicit declaration of function 'fnDMA_BufferReset' [-Wimplicit-function-declaration]&lt;BR /&gt; fnDMA_BufferReset(9, DMA_BUFFER_START);&lt;BR /&gt; ^~~~~~~~~~~~~~~~~&lt;BR /&gt;../source/pit.c:437:26: error: 'DMA_BUFFER_START' undeclared (first use in this function); did you mean 'DMA_CSR_START'?&lt;BR /&gt; fnDMA_BufferReset(9, DMA_BUFFER_START);&lt;BR /&gt; ^~~~~~~~~~~~~~~~&lt;BR /&gt; DMA_CSR_START&lt;BR /&gt;../source/pit.c: In function 'main':&lt;BR /&gt;../source/pit.c:860:18: warning: unused variable 'pitConfig' [-Wunused-variable]&lt;BR /&gt; pit_config_t pitConfig;&lt;BR /&gt; ^~~~~~~~~&lt;BR /&gt;At top level:&lt;BR /&gt;../source/pit.c:418:13: warning: 'fnSampleBus' defined but not used [-Wunused-function]&lt;BR /&gt; static void fnSampleBus(void)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Nov 2018 14:26:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797794#M48536</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2018-11-24T14:26:47Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797795#M48537</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I think you're working with KDS, and the libraries may be different from the ones used by MCUXpresso.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I have opened MCUXpresso, and in the "Pins" option, it seems that I can assign a DMA interrupt to the input ports, maybe this will configure me the same but using the MCUXpresso libraries. Problem is that need enabled and configured interrupt DMA and the Peripheral Tools seem its not available for Kinetis MK66, so need codify manually.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/77818i1296E5DA32CFBDC5/image-size/large?v=v2&amp;amp;px=999" title="ScreenHunter_014.jpg" alt="ScreenHunter_014.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/77868i8B9F866561A64E4B/image-size/large?v=v2&amp;amp;px=999" title="ScreenHunter_011.jpg" alt="ScreenHunter_011.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Nov 2018 14:43:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797795#M48537</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2018-11-24T14:43:14Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797796#M48538</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Luis&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. The DMA controller supports an interrupt on either half or full buffer completion. If it were to interrupt on each DMA transfer it would not really have any advantage over interrupts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. In DMA mode the sources trigger the DMA transfer but there is no way to know which one it was (also, without interrupts, one doesn't necessarily know that it has taken place)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. I set up for continuous operation but&lt;/P&gt;&lt;PRE class=""&gt;&lt;CODE&gt;&lt;SPAN class=""&gt;fnDMA_BufferReset&lt;/SPAN&gt;&lt;SPAN class=""&gt;(&lt;/SPAN&gt;&lt;SPAN class=""&gt;9&lt;/SPAN&gt;&lt;SPAN class=""&gt;,&lt;/SPAN&gt; DMA_BUFFER_STOP&lt;SPAN class=""&gt;)&lt;/SPAN&gt;&lt;SPAN class=""&gt;;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;can be used to stop it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From your latest information I think that &lt;STRONG&gt;interrupt driven&lt;/STRONG&gt; operation is the most suitable for you. This is the code that does it in the uTasker project. I also attached a further video to show how it is verified.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; __callback_interrupt &lt;SPAN class="token function"&gt;irq_control_change&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; iInputRef&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; ucData &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;_READ_PORT&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;C&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;gt;&amp;gt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;16&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// read the data bus (PTC23..PTC16)&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;switch&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;iInputRef&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;case&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;16&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// PTB16&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ucData &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; ucData&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;break&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;case&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;17&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// PTB17&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ucData &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; ucData&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;break&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;case&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;18&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// PTB18&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ucData &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; ucData&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;break&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;case&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;19&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// PTB19&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ucData &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; ucData&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;break&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;case&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;20&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// PTB20&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ucData &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; ucData&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;break&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;case&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;21&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// PTB21&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ucData &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; ucData&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;break&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;


&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;fnConfigureBus&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; INTERRUPT_SETUP interrupt_setup&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// interrupt configuration parameters&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;int_type &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; PORT_INTERRUPT&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// identifier to configure port interrupt&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;int_port &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; PORTB&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// the port that the interrupt input is on&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;int_port_bits &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;PORTB_BIT16 &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; PORTB_BIT17 &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; PORTB_BIT18 &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; PORTB_BIT19 &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; PORTB_BIT20 &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; PORTB_BIT21&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// UART input pin on FRDM-K64F&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;int_port_sense &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;IRQ_FALLING_EDGE &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; PULLUP_ON&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// interrupt on falling edge&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;int_handler &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; irq_control_change&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// interrupt handler on any edge&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;int_priority &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;2&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// use interrupt priority 2 for port interrupts&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;fnConfigureInterrupt&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;interrupt_setup&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// configure interrupt&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Nov 2018 14:48:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797796#M48538</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-11-24T14:48:45Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797797#M48539</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Luis&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with the uTasker code, which works in KDS, MCUXpresso, S32, CodeWarrior, Atollic, Crossworks, IAR, Keil, Green Hills, CooCox, GNU and VisualStudio.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It can be used together with the NXP framework but needs the libraries from GitHub (uTasker) to be used too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case you can only use NXP libraries you may need to rework and further develop their examples to get something similar since the uTasker hardware layer APIs encapsulate a higher level of functionality and usability on top of its Kinetis chip simulation capabilities.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that the uTasker methods make the pin configuration tools redundant (these also don't support all chips and older ones like PE are legacy and not supported any more anyway). As you can see, the uTasker API just needs to be told the pins you want to use and it does all the work for you (and will work on any other chip too without needing to port code or go through the same generation steps again each time something is changed).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Nov 2018 14:55:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797797#M48539</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-11-24T14:55:04Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis MK66, DMA to read GPIO</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797798#M48540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Mark.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Yes, as far as I understand, in this case using the DMA would not bring advantages, I would have to use common interrupts assigned to each port that should trigger the capture of the 8bit data bus in the GPIO.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I can configure the interrupts in MCUXpresso from the "Pins" tool, which generates all the source code automatically.&amp;nbsp;I just needed to know how to read the state of the 8 pins, with a single instruction, since before I did it reading one by one each pin, and also reading one by one each of the control bus pins. It was slow and did not work well, probably because the data entered faster than the program was able to read.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Now in the interrupt is already identified the signal that caused the interrupt, and with the way you have indicated me to read the 8 pins with a single instruction, I think that must work all right.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In any case, I appreciate the information about the configuration of the DMA, I'm sure it will be very useful for other programs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: seem there are may differences and compatibility problems, between KDS and MCUXpresso.&lt;/P&gt;&lt;P&gt;Greetings.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Nov 2018 15:02:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-MK66-DMA-to-read-GPIO/m-p/797798#M48540</guid>
      <dc:creator>luishs</dc:creator>
      <dc:date>2018-11-24T15:02:01Z</dc:date>
    </item>
  </channel>
</rss>