<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollersのトピックi2c transactions cause pwm glitches</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/i2c-transactions-cause-pwm-glitches/m-p/795556#M48430</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a&amp;nbsp;MKV11Z64VXX7,&amp;nbsp; and all the very latest sdk components/libraries.&amp;nbsp; (as of 6/19/18)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the device configured so that the ftms are being used to drive many independent pwm signals.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I issue a periodic i2c transaction ,&amp;nbsp; the transaction is successful,&amp;nbsp; however, I see a glitch on the&amp;nbsp;&lt;/P&gt;&lt;P&gt;pwm signals.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wondering if anyone else has see an issue&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;Nick P.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jun 2018 19:15:25 GMT</pubDate>
    <dc:creator>nick_preiser</dc:creator>
    <dc:date>2018-06-19T19:15:25Z</dc:date>
    <item>
      <title>i2c transactions cause pwm glitches</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/i2c-transactions-cause-pwm-glitches/m-p/795556#M48430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a&amp;nbsp;MKV11Z64VXX7,&amp;nbsp; and all the very latest sdk components/libraries.&amp;nbsp; (as of 6/19/18)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the device configured so that the ftms are being used to drive many independent pwm signals.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I issue a periodic i2c transaction ,&amp;nbsp; the transaction is successful,&amp;nbsp; however, I see a glitch on the&amp;nbsp;&lt;/P&gt;&lt;P&gt;pwm signals.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wondering if anyone else has see an issue&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;Nick P.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jun 2018 19:15:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/i2c-transactions-cause-pwm-glitches/m-p/795556#M48430</guid>
      <dc:creator>nick_preiser</dc:creator>
      <dc:date>2018-06-19T19:15:25Z</dc:date>
    </item>
    <item>
      <title>Re: i2c transactions cause pwm glitches</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/i2c-transactions-cause-pwm-glitches/m-p/795557#M48431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Nick,&lt;/P&gt;&lt;P&gt;The PWM signal is a digital signal, it is normal that the PWM signal has undershoot and overshoot, I do not think it take effect on anything.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jun 2018 09:46:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/i2c-transactions-cause-pwm-glitches/m-p/795557#M48431</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-06-20T09:46:41Z</dc:date>
    </item>
    <item>
      <title>Re: i2c transactions cause pwm glitches</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/i2c-transactions-cause-pwm-glitches/m-p/795558#M48432</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found that the issue only happens when I am using my jtag debugger,&amp;nbsp; under sw debug.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Under normal operation,&amp;nbsp; no issue.&amp;nbsp; I am guessing that there is some resource sharing issue betwen the&amp;nbsp; semi-hosting and the i2c/ftm/pwm...&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am going to close this for now.&amp;nbsp; thanks&amp;nbsp; Nick,&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jun 2018 14:44:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/i2c-transactions-cause-pwm-glitches/m-p/795558#M48432</guid>
      <dc:creator>nick_preiser</dc:creator>
      <dc:date>2018-06-20T14:44:28Z</dc:date>
    </item>
  </channel>
</rss>