<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32 DS new Project has .bss 2420 Bytes? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S32-DS-new-Project-has-bss-2420-Bytes/m-p/795012#M48412</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am trying to create a project in S32 design studio for arm (KEAZN64, 4K SRAM). but i have the problem that the project is still empty and i just have the main.cpp file (empty) but the .bss section is about 2,5KB? the MCU has only 4KB SRAM and i do not have any thing till now in the source code. i am also using the library ewl_c++_no_IO but i really do not need it, but if i set the library selection on none, i get alot of erros?!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;any suggestions please?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance.&lt;/P&gt;&lt;P&gt;Hani&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Sep 2018 14:48:15 GMT</pubDate>
    <dc:creator>hanisamara</dc:creator>
    <dc:date>2018-09-25T14:48:15Z</dc:date>
    <item>
      <title>S32 DS new Project has .bss 2420 Bytes?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S32-DS-new-Project-has-bss-2420-Bytes/m-p/795012#M48412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am trying to create a project in S32 design studio for arm (KEAZN64, 4K SRAM). but i have the problem that the project is still empty and i just have the main.cpp file (empty) but the .bss section is about 2,5KB? the MCU has only 4KB SRAM and i do not have any thing till now in the source code. i am also using the library ewl_c++_no_IO but i really do not need it, but if i set the library selection on none, i get alot of erros?!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;any suggestions please?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance.&lt;/P&gt;&lt;P&gt;Hani&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 14:48:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S32-DS-new-Project-has-bss-2420-Bytes/m-p/795012#M48412</guid>
      <dc:creator>hanisamara</dc:creator>
      <dc:date>2018-09-25T14:48:15Z</dc:date>
    </item>
    <item>
      <title>Re: S32 DS new Project has .bss 2420 Bytes?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S32-DS-new-Project-has-bss-2420-Bytes/m-p/795013#M48413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hani,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in the project linker file, there is by default set heap size to 0x500 and stack size 0x400, which causes, almost 2,5Kb of memory is reserved.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend you to shrink these two areas (heap size can be 0 in case you do not use dynamic memory allocation or some similar features), stack size depends on your application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73864i4D12918C27CF38D5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Oct 2018 12:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S32-DS-new-Project-has-bss-2420-Bytes/m-p/795013#M48413</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2018-10-04T12:31:25Z</dc:date>
    </item>
  </channel>
</rss>