<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MK30D10 (100MHZ) FlexCAN issue in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK30D10-100MHZ-FlexCAN-issue/m-p/794458#M48382</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Tatlinar,&lt;/P&gt;&lt;P&gt;Pls refer to the section in RM of K30, I copy it here:&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;3.9.1.3 Number of message buffers&lt;BR /&gt;Each FlexCAN module contains 16 message buffers. Each message buffer is 16 bytes.&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;It means that the RAM size is 16* 16=256 bytes.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Jul 2018 09:30:18 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2018-07-11T09:30:18Z</dc:date>
    <item>
      <title>MK30D10 (100MHZ) FlexCAN issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK30D10-100MHZ-FlexCAN-issue/m-p/794457#M48381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was trying to use RX Fifo for K30D10 FlexCan module. Reference manual says there is 64 MB could be use and up to 128 Fifo Filter could be use. But, I realized that I cannot use more then 16 MB. I could not reach CS16 register in example. At CTRL2[RFFN] register there is a table. RFFN could be 3 maximum. But there is nothing about this limitation. Do I have to something to use full functional CAN? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jul 2018 14:05:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK30D10-100MHZ-FlexCAN-issue/m-p/794457#M48381</guid>
      <dc:creator>i_smailtatlınar</dc:creator>
      <dc:date>2018-07-09T14:05:29Z</dc:date>
    </item>
    <item>
      <title>Re: MK30D10 (100MHZ) FlexCAN issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK30D10-100MHZ-FlexCAN-issue/m-p/794458#M48382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Tatlinar,&lt;/P&gt;&lt;P&gt;Pls refer to the section in RM of K30, I copy it here:&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;3.9.1.3 Number of message buffers&lt;BR /&gt;Each FlexCAN module contains 16 message buffers. Each message buffer is 16 bytes.&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;It means that the RAM size is 16* 16=256 bytes.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jul 2018 09:30:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK30D10-100MHZ-FlexCAN-issue/m-p/794458#M48382</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-07-11T09:30:18Z</dc:date>
    </item>
  </channel>
</rss>