<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: MK20DN512ZVMC10 USB Host enumeration problem.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DN512ZVMC10-USB-Host-enumeration-problem/m-p/158021#M483</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello. &lt;/P&gt;&lt;P&gt;The answer is correct, I added MPU_CESR = 0; and it works, but I have another problem, when I debug everything works correctly. but off the debugger and the USB is not working. Why can this happen?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Feb 2014 08:35:16 GMT</pubDate>
    <dc:creator>fernandogarcia</dc:creator>
    <dc:date>2014-02-26T08:35:16Z</dc:date>
    <item>
      <title>MK20DN512ZVMC10 USB Host enumeration problem.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DN512ZVMC10-USB-Host-enumeration-problem/m-p/158019#M481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We've created a product on base of MK20DN512ZVMC10 and set it up properly on software level. Although, it doesn't enumerate any USB device connected to the USB port. The register TXSUSPENDTOKENBUSY is set to 1 right after the first setup packet sent over USB. SOF packets get generated and their transmission is going on over D+ and D-.&lt;/P&gt;&lt;P&gt;The code from khci.c which is makes this happen is following:&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;case TR_CTRL:&amp;nbsp; &lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;bd_ptr = (uint_32*) BD_PTR(0, 1, usb_host_ptr-&amp;gt;tx_bd);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;*(bd_ptr + 1) = HOST_TO_LE_LONG((uint_32)buf);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;*bd_ptr = HOST_TO_LE_LONG(USB_BD_BC(len) | USB_BD_OWN);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp; ------&amp;gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;usb_ptr-&amp;gt;TOKEN = (uint_8)(USB_TOKEN_TOKENENDPT((uint_8)pipe_desc_ptr-&amp;gt;G.ENDPOINT_NUMBER) | USB_TOKEN_TOKENPID_SETUP);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;usb_host_ptr-&amp;gt;tx_bd ^= 1;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;break;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We've tried to run the software from RAM and from FLASH with no results. We have 2.2pF on VOUT33 so recommendations from other posts do not work. We have tested it with 3 different configurations: added external mouse, external hub, and our internal hub. The same code with the same equipment works fine on TWR-K53. We are using 8MHz external oscillator. Source code for initialization of clocks are in attachment.&lt;/P&gt;&lt;P&gt;Please, help to locate a problem ASAP.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Oct 2012 11:37:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DN512ZVMC10-USB-Host-enumeration-problem/m-p/158019#M481</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2012-10-30T11:37:29Z</dc:date>
    </item>
    <item>
      <title>Re: MK20DN512ZVMC10 USB Host enumeration problem.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DN512ZVMC10-USB-Host-enumeration-problem/m-p/158020#M482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem is in missing initialization register.&lt;/P&gt;&lt;P&gt;Add &lt;/P&gt;&lt;P&gt;MPU_CESR=0; &lt;/P&gt;&lt;P&gt;before return from pll_init() function.&lt;/P&gt;&lt;P&gt;Also, make sure that you switch to external reference clocks.&lt;/P&gt;&lt;P&gt;MCG_C1 = MCG_C1_CLKS(2) | MCG_C1_FRDIV(3);&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Nov 2012 18:34:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DN512ZVMC10-USB-Host-enumeration-problem/m-p/158020#M482</guid>
      <dc:creator>akvarel</dc:creator>
      <dc:date>2012-11-03T18:34:47Z</dc:date>
    </item>
    <item>
      <title>Re: MK20DN512ZVMC10 USB Host enumeration problem.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DN512ZVMC10-USB-Host-enumeration-problem/m-p/158021#M483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello. &lt;/P&gt;&lt;P&gt;The answer is correct, I added MPU_CESR = 0; and it works, but I have another problem, when I debug everything works correctly. but off the debugger and the USB is not working. Why can this happen?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2014 08:35:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DN512ZVMC10-USB-Host-enumeration-problem/m-p/158021#M483</guid>
      <dc:creator>fernandogarcia</dc:creator>
      <dc:date>2014-02-26T08:35:16Z</dc:date>
    </item>
  </channel>
</rss>