<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: FRDM-KL28Z Keil uVision</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL28Z-Keil-uVision/m-p/793169#M48246</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply Victor, and sorry for the delayed response.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've checked that the correct pack is installed, I see the same as your picture.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I do not see the connected board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Its plugged in through the SDA port and the light is on.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using firmware from SEGGER&lt;/P&gt;&lt;P&gt;The J-Link OpenSDA Board specific firmware,&amp;nbsp;FRDM-KL28Z.&lt;/P&gt;&lt;P&gt;Can you link to link to the firmware you're using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74893i0ECF160701A56DEC/image-size/large?v=v2&amp;amp;px=999" title="packinstaller.png" alt="packinstaller.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74958iDEAA1B2BDD9E04BE/image-size/large?v=v2&amp;amp;px=999" title="jlink.png" alt="jlink.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Nov 2018 20:50:51 GMT</pubDate>
    <dc:creator>mjk29</dc:creator>
    <dc:date>2018-11-14T20:50:51Z</dc:date>
    <item>
      <title>FRDM-KL28Z Keil uVision</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL28Z-Keil-uVision/m-p/793167#M48244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am attempting to develop a project on a FRDM-KL28Z board using Keil uVision.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am running into difficulties connecting to the board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I attempt to setup the connection to my board in uVision I see the following.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board is connected through its open SDA USB port.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am able to see the connected volume through windows explorer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can connect to the board using PUTTY.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can connect to the board using MCUXpresso.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What must I do to connect using uVision?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Nov 2018 05:19:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL28Z-Keil-uVision/m-p/793167#M48244</guid>
      <dc:creator>mjk29</dc:creator>
      <dc:date>2018-11-01T05:19:11Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL28Z Keil uVision</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL28Z-Keil-uVision/m-p/793168#M48245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Matthew Kehoe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which version of Keil uVision are you running? I tried with the newest version 5.26.2 and I didn't face any kind of problems.&lt;/P&gt;&lt;P&gt;Be sure that you have the corresponding packets installed.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66981iE19A4C71C55756AA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_7.png" alt="pastedImage_7.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Select the debug interface that you want to use depending on the firmware that you have on the OpenSDA of your FRDM, in my case is J-Link.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67058iE3A0763FE8FA43CA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_9.png" alt="pastedImage_9.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Once you select the corresponding interface click on the setting button and you should see something like the following.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67102i51103E4C9F3F65C1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_10.png" alt="pastedImage_10.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Please let me know the results on your side!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Nov 2018 21:42:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL28Z-Keil-uVision/m-p/793168#M48245</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-11-01T21:42:16Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL28Z Keil uVision</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL28Z-Keil-uVision/m-p/793169#M48246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply Victor, and sorry for the delayed response.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've checked that the correct pack is installed, I see the same as your picture.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I do not see the connected board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Its plugged in through the SDA port and the light is on.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using firmware from SEGGER&lt;/P&gt;&lt;P&gt;The J-Link OpenSDA Board specific firmware,&amp;nbsp;FRDM-KL28Z.&lt;/P&gt;&lt;P&gt;Can you link to link to the firmware you're using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74893i0ECF160701A56DEC/image-size/large?v=v2&amp;amp;px=999" title="packinstaller.png" alt="packinstaller.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74958iDEAA1B2BDD9E04BE/image-size/large?v=v2&amp;amp;px=999" title="jlink.png" alt="jlink.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2018 20:50:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL28Z-Keil-uVision/m-p/793169#M48246</guid>
      <dc:creator>mjk29</dc:creator>
      <dc:date>2018-11-14T20:50:51Z</dc:date>
    </item>
  </channel>
</rss>