<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKinetis K20 and WINUSB on windows 10</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K20-and-WINUSB-on-windows-10/m-p/791390#M48156</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a K20 based WINUSB device that fails to start automatically in Windows 10. When I plug it in it shows up in device manager under Universal Serial Bus Devices with the proper name and a question mark. When I look at the enumeration process in the USB Beagle debugger I can see that it failed. On the 3rd call to get device descriptor by the host, the device responds with an empty data packet and Windows gives up.&lt;/P&gt;&lt;P&gt;Whats strange is if I right click the device in device manager and select uninstall the device starts. It goes through a different enumeration process by making some control transfers rather than request the MS extended compatibility ID OS feature descriptor but it works.&lt;/P&gt;&lt;P&gt;If I unplug the device and plug it back in we are back to the question mark. With or without the question mark the device is using winusb.sys as the driver.&lt;/P&gt;&lt;P&gt;Any ideas as to what I might be doing wrong? This is only a problem on Windows 10 and only with a very small percentage of our devices.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Jun 2018 20:03:32 GMT</pubDate>
    <dc:creator>ryanlush</dc:creator>
    <dc:date>2018-06-18T20:03:32Z</dc:date>
    <item>
      <title>Kinetis K20 and WINUSB on windows 10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K20-and-WINUSB-on-windows-10/m-p/791390#M48156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a K20 based WINUSB device that fails to start automatically in Windows 10. When I plug it in it shows up in device manager under Universal Serial Bus Devices with the proper name and a question mark. When I look at the enumeration process in the USB Beagle debugger I can see that it failed. On the 3rd call to get device descriptor by the host, the device responds with an empty data packet and Windows gives up.&lt;/P&gt;&lt;P&gt;Whats strange is if I right click the device in device manager and select uninstall the device starts. It goes through a different enumeration process by making some control transfers rather than request the MS extended compatibility ID OS feature descriptor but it works.&lt;/P&gt;&lt;P&gt;If I unplug the device and plug it back in we are back to the question mark. With or without the question mark the device is using winusb.sys as the driver.&lt;/P&gt;&lt;P&gt;Any ideas as to what I might be doing wrong? This is only a problem on Windows 10 and only with a very small percentage of our devices.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jun 2018 20:03:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K20-and-WINUSB-on-windows-10/m-p/791390#M48156</guid>
      <dc:creator>ryanlush</dc:creator>
      <dc:date>2018-06-18T20:03:32Z</dc:date>
    </item>
  </channel>
</rss>