<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 GPIO status after power saving mode</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-status-after-power-saving-mode/m-p/790541#M48102</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, i have confused for GPIO status out of control after wake up from power saving mode(LLS3).&lt;/P&gt;&lt;P&gt;i am&amp;nbsp;coding on the MCU MKW31Z512 series.&lt;/P&gt;&lt;P&gt;before&amp;nbsp;i go to the LLS3 mode, i have configured the GPIO to output push-pull.(ex. PTA19, PTB2...etc).&lt;/P&gt;&lt;P&gt;But the GPIO will out of control for can not set high or low level when i wake up from LLS3 mode by sleep timeout&lt;/P&gt;&lt;P&gt;I must configures the pin mux again to let GPIO back to normal.&lt;/P&gt;&lt;P&gt;Is something wrong with my setting?&lt;/P&gt;&lt;P&gt;Thank you!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Sep 2018 10:12:24 GMT</pubDate>
    <dc:creator>ethanchiu</dc:creator>
    <dc:date>2018-09-04T10:12:24Z</dc:date>
    <item>
      <title>GPIO status after power saving mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-status-after-power-saving-mode/m-p/790541#M48102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, i have confused for GPIO status out of control after wake up from power saving mode(LLS3).&lt;/P&gt;&lt;P&gt;i am&amp;nbsp;coding on the MCU MKW31Z512 series.&lt;/P&gt;&lt;P&gt;before&amp;nbsp;i go to the LLS3 mode, i have configured the GPIO to output push-pull.(ex. PTA19, PTB2...etc).&lt;/P&gt;&lt;P&gt;But the GPIO will out of control for can not set high or low level when i wake up from LLS3 mode by sleep timeout&lt;/P&gt;&lt;P&gt;I must configures the pin mux again to let GPIO back to normal.&lt;/P&gt;&lt;P&gt;Is something wrong with my setting?&lt;/P&gt;&lt;P&gt;Thank you!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Sep 2018 10:12:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-status-after-power-saving-mode/m-p/790541#M48102</guid>
      <dc:creator>ethanchiu</dc:creator>
      <dc:date>2018-09-04T10:12:24Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO status after power saving mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-status-after-power-saving-mode/m-p/790542#M48103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using Connectivity software to get into LLS mode? I would like to recommend you to check the Application note:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.freescale.com/files/32bit/doc/app_note/AN4503.pdf" title="http://cache.freescale.com/files/32bit/doc/app_note/AN4503.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4503.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN5088.pdf" title="https://www.nxp.com/docs/en/application-note/AN5088.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN5088.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to Reference Manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;When in LLS mode, the I/O pins are held in their input or output state.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Upon wakeup, the PMC is re-enabled, goes through a &lt;/EM&gt;power up&lt;EM&gt; sequence to full&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;regulation, and releases the logic from state retention mode. The I/O are released&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;immediately after a wake-up or reset event. In the case of LLS exit via a RESET pin, the&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;I/O default to their reset state.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this could help you.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 22:21:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-status-after-power-saving-mode/m-p/790542#M48103</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2018-09-05T22:21:01Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO status after power saving mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-status-after-power-saving-mode/m-p/790543#M48104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ethan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG style="font-size: 12px; font-family: courier new, courier, monospace;"&gt;PMC_REGSC = PMC_REGSC_ACKISO; // acknowledge the isolation mode to set certain peripherals and I/O pads back to normal run state&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3366ff;"&gt;&lt;EM&gt;uTasker - for more performance and faster, cheaper product development&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 22:58:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-status-after-power-saving-mode/m-p/790543#M48104</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-09-05T22:58:10Z</dc:date>
    </item>
  </channel>
</rss>