<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックSPI TX FiFo is not sending data out</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-TX-FiFo-is-not-sending-data-out/m-p/788340#M47996</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem with the SPI communication concerning the TX FIFO. I try to send 3 words through fifo without waiting active on the TCF flag afterwards, but handle in incoming data when the RX FIFO countains 3 words. So what I have done is to enable the FIFO and write three bytes with push. I have enabled the Interrupt Request Selects for TCF but the ISR is not called. When I have a look with in the registers from Debugger I see that data is not send out, but the Fifo counter is still 3. So is there anything I'm missing why data is kept in fifo in and not sent?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Dec 2018 11:56:32 GMT</pubDate>
    <dc:creator>christophosterl</dc:creator>
    <dc:date>2018-12-12T11:56:32Z</dc:date>
    <item>
      <title>SPI TX FiFo is not sending data out</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-TX-FiFo-is-not-sending-data-out/m-p/788340#M47996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem with the SPI communication concerning the TX FIFO. I try to send 3 words through fifo without waiting active on the TCF flag afterwards, but handle in incoming data when the RX FIFO countains 3 words. So what I have done is to enable the FIFO and write three bytes with push. I have enabled the Interrupt Request Selects for TCF but the ISR is not called. When I have a look with in the registers from Debugger I see that data is not send out, but the Fifo counter is still 3. So is there anything I'm missing why data is kept in fifo in and not sent?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2018 11:56:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-TX-FiFo-is-not-sending-data-out/m-p/788340#M47996</guid>
      <dc:creator>christophosterl</dc:creator>
      <dc:date>2018-12-12T11:56:32Z</dc:date>
    </item>
    <item>
      <title>Re: SPI TX FiFo is not sending data out</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-TX-FiFo-is-not-sending-data-out/m-p/788341#M47997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi christophosterloh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for my late reply!&lt;/P&gt;&lt;P&gt;Not sure about your MCU part number.(Seem that you are using K27)&lt;BR /&gt;Have you try to test the SPI example in latest &lt;A href="https://mcuxpresso.nxp.com/en/select"&gt;MCUXPresso SDK&lt;/A&gt;_2.4.1_MK27FN2M0Axxx15?&lt;/P&gt;&lt;P&gt;(...\SDK_2.4.1_MK27FN2M0Axxx15\boards\frdmk28fa\driver_examples\dspi)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Dec 2018 08:22:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-TX-FiFo-is-not-sending-data-out/m-p/788341#M47997</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2018-12-14T08:22:23Z</dc:date>
    </item>
  </channel>
</rss>