<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 clock amplitude inquiry on 32kHz crystal</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/clock-amplitude-inquiry-on-32kHz-crystal/m-p/787837#M47952</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using Kinetis K81 family mcu.&lt;/P&gt;&lt;P&gt;In the specification for the 32kHz clock for EXTAL32 , it was specified that the typical peak-to-peak amplitude of oscillation is 0.6V and no tolerance was given.&lt;/P&gt;&lt;P&gt;My actual measurement on the amplitude is 0.55V.&amp;nbsp; &amp;nbsp;I would like to ask if this will normally work or what voltage range should be I'm looking at.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Aug 2018 01:50:26 GMT</pubDate>
    <dc:creator>darwin_deramos</dc:creator>
    <dc:date>2018-08-16T01:50:26Z</dc:date>
    <item>
      <title>clock amplitude inquiry on 32kHz crystal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/clock-amplitude-inquiry-on-32kHz-crystal/m-p/787837#M47952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using Kinetis K81 family mcu.&lt;/P&gt;&lt;P&gt;In the specification for the 32kHz clock for EXTAL32 , it was specified that the typical peak-to-peak amplitude of oscillation is 0.6V and no tolerance was given.&lt;/P&gt;&lt;P&gt;My actual measurement on the amplitude is 0.55V.&amp;nbsp; &amp;nbsp;I would like to ask if this will normally work or what voltage range should be I'm looking at.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 01:50:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/clock-amplitude-inquiry-on-32kHz-crystal/m-p/787837#M47952</guid>
      <dc:creator>darwin_deramos</dc:creator>
      <dc:date>2018-08-16T01:50:26Z</dc:date>
    </item>
    <item>
      <title>Re: clock amplitude inquiry on 32kHz crystal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/clock-amplitude-inquiry-on-32kHz-crystal/m-p/787838#M47953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the data sheet, there has a specification on the 32kHz OSC:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67144i90A2B47C991B5C81/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Aug 2018 08:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/clock-amplitude-inquiry-on-32kHz-crystal/m-p/787838#M47953</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2018-08-21T08:33:05Z</dc:date>
    </item>
  </channel>
</rss>