<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: EZP Port issue</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/EZP-Port-issue/m-p/787640#M47937</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anna,&lt;/P&gt;&lt;P&gt;First, if you clear FOPT[EZPORT_DIS], chip will not enter EZPORT mode. You can't program FLASH at any time.&lt;BR /&gt;If you connet EZP_CS to ground, you can't send SPI command. "The negation of EZP_CS indicates that the current command has finished and resets the EzPort state machine, so that EzPort is ready to receive the next command."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Sep 2018 05:31:57 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2018-09-25T05:31:57Z</dc:date>
    <item>
      <title>EZP Port issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/EZP-Port-issue/m-p/787639#M47936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i am using the micro MK22FN512, and the gpio EZP_CS is put to GND. In this condition on the power on the micro goes in the EZPORT mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have found a solution to avoid this behaviour -&amp;gt; disable the EZ register on the FOTP (0x40D) using the SPI protocol.&lt;/P&gt;&lt;P&gt;The question is: Can i send the right command sequence&lt;/P&gt;&lt;P&gt;* WRITE_ENABLE CMD&lt;/P&gt;&lt;P&gt;*ERASE THE SECTOR CMD (0x00)&lt;/P&gt;&lt;P&gt;* WAIT THE SE REGISTER IS SET&lt;/P&gt;&lt;P&gt;*WRITE_ENABLE CMD&lt;/P&gt;&lt;P&gt;*PROGRAM ADDRESS CDM (0X40D0&lt;/P&gt;&lt;P&gt;*WAIT THE SE REGISTER IS SET&lt;/P&gt;&lt;P&gt;if the EZP_CS is put to ground during the sequence? Or is it necessary handle it and have a falling edge before send a command?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;-Anna&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Sep 2018 21:21:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/EZP-Port-issue/m-p/787639#M47936</guid>
      <dc:creator>anna_palumbo</dc:creator>
      <dc:date>2018-09-21T21:21:42Z</dc:date>
    </item>
    <item>
      <title>Re: EZP Port issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/EZP-Port-issue/m-p/787640#M47937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anna,&lt;/P&gt;&lt;P&gt;First, if you clear FOPT[EZPORT_DIS], chip will not enter EZPORT mode. You can't program FLASH at any time.&lt;BR /&gt;If you connet EZP_CS to ground, you can't send SPI command. "The negation of EZP_CS indicates that the current command has finished and resets the EzPort state machine, so that EzPort is ready to receive the next command."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 05:31:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/EZP-Port-issue/m-p/787640#M47937</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2018-09-25T05:31:57Z</dc:date>
    </item>
  </channel>
</rss>