<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: target initiallization failed in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/target-initiallization-failed/m-p/786926#M47888</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hemanth K, &lt;/P&gt;&lt;P&gt;How about programming a simple project ? And can it debug well using the debugger ?&lt;/P&gt;&lt;P&gt;If still can't work , please check debug configration and flash program configurations:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69613i594F4E8D80A88351/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Sep 2018 05:25:46 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2018-09-25T05:25:46Z</dc:date>
    <item>
      <title>target initiallization failed</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/target-initiallization-failed/m-p/786925#M47887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using Codewarrior 10.6 trial version. We have a board with "MK61FN1M0VMJ12" microcontroller. There is a problem while programming with Universal Mutilink 2.0.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The error while launching Internal flash configuration is as follows:&lt;/P&gt;&lt;P&gt;___________________________________________________________&lt;/P&gt;&lt;P&gt;fl::target -lc "LC for Simple Flash"&lt;BR /&gt;fl::target -b 0x1fff0000 0x20000&lt;BR /&gt;fl::target -v off -l off&lt;BR /&gt;cmdwin::fl::device -d "FTFE_PFlash1M0" -o "128Kx64x1" -a 0x0 0xfffff&lt;BR /&gt;cmdwin::fl::image -f "E:\\CW_WORKSPACE\\DCC_03082017_bel demo final\\MK70FN1M0_INTERNAL_FLASH\\Aslesha_Card_Test.afx" -t "Auto Detect" -re on -r 0x0 0xfffff -oe off&lt;BR /&gt;cmdwin::fl::erase image&lt;BR /&gt; Beginning Operation ... &lt;BR /&gt;------------------------- &lt;BR /&gt;Auto-detection is successful. &lt;BR /&gt; File is of type Elf Format. &lt;BR /&gt; &lt;BR /&gt;Performing target initialization ... &lt;BR /&gt;Error: Connect Failed.&lt;BR /&gt;Can't connect. The Debugger can not connect to the P&amp;amp;E device(ARM GDI Protocol Adapter)&lt;BR /&gt;Error: Connect Failed.&lt;/P&gt;&lt;P&gt;____________________________________________________________________________________&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Earlier, we have tried to do the same process with CW 11, 10.7 versions also but no success could be achieved. We encountered the same error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PLEASE REPLY ASAP.&lt;/P&gt;&lt;P&gt;WE ARE STUCK WITH THIS ERROR IN MIDDLE OF A PROJECT.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Hemanth K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Sep 2018 08:39:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/target-initiallization-failed/m-p/786925#M47887</guid>
      <dc:creator>hemanth_kl</dc:creator>
      <dc:date>2018-09-22T08:39:04Z</dc:date>
    </item>
    <item>
      <title>Re: target initiallization failed</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/target-initiallization-failed/m-p/786926#M47888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hemanth K, &lt;/P&gt;&lt;P&gt;How about programming a simple project ? And can it debug well using the debugger ?&lt;/P&gt;&lt;P&gt;If still can't work , please check debug configration and flash program configurations:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69613i594F4E8D80A88351/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 05:25:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/target-initiallization-failed/m-p/786926#M47888</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-09-25T05:25:46Z</dc:date>
    </item>
  </channel>
</rss>